STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1567 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 595 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

STM32cubeIDE

we are trying to execute the CAN messages here we get error we are added header files but it give same errorplease tell me how to resolve that error we are waiting for your information thank youthanks and regards,B.Mahaboob Shareef.

Can't build project after re-installing CubeIDE

After re-installing Ubuntu on my laptop and installing CubeIDE v12.1 I can't build a previously building project and get the error:`make: *** No rule to make target '/home/shane/Desktop/STM32Cube/Repository/STM32Cube_FW_F3_V1.11.4/Drivers/STM32F3xx_H...

STM32F446 ADC permanent conversion by polling?

Hi,I want to read analogue values out of the ADC of an STM32F446. This works well when using CubeMX-based functions.The initialisation:   hadc1.Instance = ADC1; hadc1.Init.ClockPrescaler = ADC_CLOCK_SYNC_PCLK_DIV4; hadc1.Init.Resolution = ADC_RE...

Resolved! Differences between debug mode and normal running

Hi all,I have a piece of code that does DMA on a UART port. This DMA i read in an buffer and i reply in 1 msSometimes i dont get the incomming UART message. I wanted to confimr this with the debug mode and reading the buffer with "live expressions". ...

Resolved! Buggy SystemClock_Config()

I use STM32CubeIDE 1.13.0 to generate code for NUCLEO-L476RG.The generated SystemClock_Config() put flash latency configuration after the clock configuration. I don't know why it works for the first call, but if I call it after exiting stop mode, it ...

nicolas by Senior II
  • 2764 Views
  • 4 replies
  • 0 kudos

Resolved! has no explicit encoding set warning

"CUBE IDE" İLE projesinde aşağıdaki hataya düştüğünde, ne anlaşılmayacağına dair bir bilgi yok. Bana bu konuda yardım eder misin? error: "'LOARA_TX_RX_end' projesinde açık bir yerleşim seti yok."proje Adı > 'LOARA_TX_RX_end'

fog.1 by Associate III
  • 40444 Views
  • 2 replies
  • 10 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.