STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1436 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 560 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

code stop in function HAL_I2C_IsDeviceReady

Hello, I am trying to use the LORA-E5 STM32WLE5JC board with the BME688 sensor, I2C connection. I used this repository as the basis GitHub - Squieler/BME68x-STM32-HAL: BME68x STM32 HAL Library, changing what was needed. But it always hangs in that ro...

Resolved! Not able to program STM32-L152RE

Hello everyone, I work in a team where we manufacture an electric car. We currently use Arduino Mega as our ECU, but we want to shift to STM. We already have a STM32-L152RE Nucleo board. I am not able to run any sort of program on the board. The code...

STM32CubeMX version issue in STM32CubeIde

Hello,I got below error while opening .ioc file in cubeIde. Invalid Input: 'project_Test.ioc' file content is not supported.This file has been generated with STM32CubeMX version '6.8.1'.Your current STM32CubeMX version is '6.8.0'.Please check for upd...

Nsg1987 by Senior
  • 5255 Views
  • 3 replies
  • 0 kudos

Stm32cubeMX where all the middleware and software package ???

Hello everyone,Is it only me, the v6.9.1 of stm32cubeMX missing a lot of middleware and software package, I try do downgrade to v6.9.0 and v6.8.1 same problem. Something broken? I builded a project and wanted to update some configuration and got this...

CubeMX_bug_v6.9.0_v6.9.1.png
SGrot.1 by Associate II
  • 1441 Views
  • 1 replies
  • 1 kudos

Timer(32bit) Inputcapture

STM32H745i Discovery kit :In this board TIM2/5 are 16/32 bit  timers when am going to configure in cubeIDE there Prescalar is 16bit  . How can  i use 32bit timer ??  and in this board input pin terminations are very crucial  ?? Any help would be than...

SA  V.1 by Senior
  • 2822 Views
  • 2 replies
  • 0 kudos

STM32 Cube IDE Update Not Working

Hi, I am working on a collaborative project. Someone sent me a new version using an updated version of STM32Cube IDE, and now the .IOC throws an error when I try to open it:To fix this, I try running Help > Check For Updates, but this gives me the fo...

image.png image (1).png Screenshot 2023-08-08 at 5.40.10 PM.png
EPala.2 by Senior
  • 3254 Views
  • 2 replies
  • 1 kudos