STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1698 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 636 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

Brain-dead STM32CubeIDE?

My laptop died so I scrambled and got another laptop up and running.  I went from the i9 to the i5.  I used to have STM32CubeIDE 1.18 which worked just fine.  I installed it and STM32CubePrg.  It built code just fine. On my "new" laptop I downloaded ...

warm38 by Associate III
  • 522 Views
  • 1 replies
  • 0 kudos

Cube IDE v2.0.0 - Hard Fault error

Hello,I had developed my firmare in STM Cube ide 1.5.1 (stm32h7/)Project repo is here: https://github.com/silelis/MustangRadio_develepementVersion/tree/main/02_Firmware/02_STM32/Radio_mainAnd after I have updated IDE to 2.0.0 I have noticed that STM3...

silelis by Associate II
  • 1479 Views
  • 15 replies
  • 5 kudos

Resolved! Stm32CubeIDE Default Setting ?

Is there an option in the STM32CubeIDE settings to reset to factory settings or something like “Default Settings”?I can’t restore the console window to its original state. When I compile the code, the console window used to appear at the bottom, but ...

XooM by Senior
  • 843 Views
  • 4 replies
  • 6 kudos

stm32fxxx_hal.h library

Hi, So i am using STM32CubeIDE to program my STM32 card, except that when i create my project, it doesnt generate an MX file. So when i try to include the library "stm32fxxx_hal.h", it doesn't work. Why is that? And am I obliged to work with STM32Cub...

Lin_Me by Associate II
  • 1722 Views
  • 15 replies
  • 10 kudos

Cannot find the specified linker script

OS : Ubuntu 24.04 LinuxTarget MCU: STM32F103CI'm new to using STM32CUBEIDE I have noticed when i created the C/C++ project and chose the target MCU something off maybe that is the issuefind the photo down below.I have added an app directory only app/...

Screenshot from 2025-12-13 16-10-45.png ziadAhmed19_0-1765635245469.png

Resolved! Regarding X-cube-ai, Cube MX, STM32cubeide v2.0.0

Sir, I have installed stm32cubeide 2.0.0 which is latest version. I opened cube mx and created a new project and selected new x cube ai package and generated the code, works fine and done successfully.after that i press exit the project, then i open ...

Resolved! CubeIDE 2.0 does not open .ioc files

Hello,Has the integrated support for CubeMX been removed in the new CubeIDE?I just updated to the latest (2.0) and now, when clicking on the ioc file of a project (created with previous version 1.19), CubeMX opens up.The top right corner has also cha...

Dega_0-1763486445192.png
Dega by Associate
  • 11223 Views
  • 16 replies
  • 37 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.