STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1555 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 589 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

Resolved! CubeIde keeps creating old workspace folder

When I first installed CubeIde I specified a workspace, but after some time I changed worspace folder. Now i want to delete that folder, btu when I do so, CubeIde creates it again.I looked into Startup and Shutdown -> Workspaces and I have there only...

UA.2 by Associate
  • 4449 Views
  • 3 replies
  • 1 kudos

How are you suposed to replicate a project???

It's a pretty common need in an IDE to be able to branch or "fork" a project. Normall, I'd make a copy of the projet at the file level, then rename the original and continue development on that. However, Ranaming a project not only crashes, but also ...

sgordon777_0-1703350703203.png

CMSIS-DSP PID help

I'm using the stm32f429 discovery, I made a PWM control and tested it with a potentiometer and it worked as expected with 1mhz. Now I need to do the temperature control, I'm using a MAX31865 with PT100 and heating a resistance with the PWM output (th...

Resolved! receive and send file in stm32f429zi

I want to send a file from terminal tool to stm32f429zi via RS485(USB to RS485 and transceiver) and store the received file in stm32F429zi board and again send it back to terminal tool and i want to know ,is it possible or not? and its not possible, ...

Live expressions in low power mode

Hi everyone,I am using a STM32L431 in my project and I am running into an unexpected behavior when debugging it. For context, I have an enum variable (lets say x_state) that represents different states in the logic. I have added this variable to the ...

dev_easyli_0-1701942065077.png dev_easyli_1-1701942462812.png dev_easyli_2-1701942689694.png

PWM TIM15 CH2 CCR1/CCR2 STM32CUBEIDE

Hello guysMy microcontroller is: STM32L432KCU6 - nucleo boardI have a problem with PWM. I need to change TIM16 to TIM15 because TIM16 collides with I2CSo thats why I have to use TIM15... I need him to handle micro servo. When i use TIM16, everything ...

conflict.jpg tiim.png clock.jpg jadupce.png
grzeniux by Associate II
  • 3671 Views
  • 5 replies
  • 3 kudos

STM32CubeIDE 1.14.0 released

STM32CubeIDE 1.14.0 was released today on st.com as well as an in-tool update patch. What is new in 1.14.0? Added the support for new microcontrollers in the STM32WB seriesAdded the support for two new boards related to the STM32WB series: NUCLEO-WBA...

Resolved! Folder in Project Explorer

Is there a possibility to create folders in which to place projects in order to better visually organize all those in the workspace?For example in the picture below there is only a small part of the long list of my projects in "Project Explorer" ... ...

luke514_0-1704312407070.png
luke514 by Senior
  • 5151 Views
  • 5 replies
  • 2 kudos