Skip to main content
Semer CHERNI
ST Employee
November 23, 2023
Question

STM32CubeIDE 1.14.0 released

STM32CubeIDE 1.14.0 was released today on st.com as well as an in-tool update patch.

  • What is new in 1.14.0?
    • Added the support for new microcontrollers in the STM32WB series
    • Added the support for two new boards related to the STM32WB series: NUCLEO-WBA55CG and STM32WBA55G-DK1
    • Added the support for a new board related to the STM32U5 series: STEVAL-MKBOXPRO
    • Added the support for STM32CubeMP13: bare-metal firmware for the STM32MP13xx
      microprocessors
    • Updated to Eclipse® 2023-09
    • GCC 12 is available on the Eclipse® p2 update site
  • Main fixed issues:
This topic has been closed for replies.

14 replies

Senior II
November 23, 2023

@Semer CHERNI  maybe you want to complete the fixed issues and known issues/limitations section by adding the link to the wiki?

When this account seems to be inactive, try @tdecker2 - ST can't change mail addresses, so I had to create a new account.
Semer CHERNI
ST Employee
November 23, 2023

Hello @t.decker 

Thanks for mentioning it :).

I made the updates.

KR,
Semer.

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
jhi
Senior
November 29, 2023

@Semer CHERNI The hard-coded keyboard shortcut to login (alt+L) is still there on 1.14.0. This gives the problem on Mac, that you are not able to type @ (on Apple QWERTZ-keyboard). Please make this configurable!

JHi

olezhandr
Associate III
December 5, 2023

Hi, It would be great to add new button in Help menu "Report STM32CubeIDE bugs"... It is not clear where the customer can get a suuport

HDaji.1
Senior
December 6, 2023

I have been using 1.7.0 from my F411 project.

Recently I downloaded and installed 1.14.0, only to find it cannot compile my 1.7.0 project.

Is it normal? How to make it work or shall I just stick with 1.7.0 IDE?

Pavel A.
December 6, 2023

@HDaji.1 Yes this is normal. Change is a curse, as a Chinese proverb says, and it is inevitable.

This is a technical forum, if something does not work after upgrade, please share relevant details.

 

HDaji.1
Senior
December 6, 2023

@Pavel A. 

Thx for the advice.

After I checked carefully, the errors are related to some shared variables, which I put in main.h.

Compiling is OK; just ld complains multiple definitions in IDE 14; strangely IDE 7 does not.

olezhandr
Associate III
December 11, 2023

After updating the ST link firmware, it refuses to detect the target and bricked two original debuggers. Don't update the firmware. Before the firmware update st-link worked

olezhandr
Associate III
December 11, 2023

olezhandr_0-1702287208645.png

 

olezhandr
Associate III
December 11, 2023

Discovery F4, Stlink V2 like soap, not whistle. I have almost delete and install STM32CubevIDE and now discovery works

Pavel A.
December 11, 2023

@olezhandr More details, please?  white ST-LINK v2 dongle or a "whistle"?

oeliks
Associate III
January 5, 2024

Hi! Is it possible for Your team to make appimage for Linux users to download?

 

Its simple, reliable and quite popular way to run Linux apps.

 

Thanks !