STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1554 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 588 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

Resolved! NUCLEO-G0B1RE and USB HID function

Hi,I would like to enable the USB HID Device function to the target uC of the NUCLEO board. So I've created a new project, selected the board and added the 2 USB pin configuration:I've also enabled the middleware functions:the clock config seems to b...

BRonc1_0-1705677489698.png BRonc1_1-1705677509499.png BRonc1_2-1705677570198.png BRonc1_3-1705677632449.png
BRonc.1 by Associate III
  • 1985 Views
  • 1 replies
  • 0 kudos

Resolved! STM32CubeIde Failed to start GDB Server on STM32F103C8

hello,I have the same problem posted by H.Ahmed on October 2022, read also in other posts:"Failed to start GDB Server Error Initializing ST-LINK deviceReason (18) Could not verify ST device!"I tried all suggestions found on web, but no help.I'm using...

Mauri by Associate II
  • 20157 Views
  • 12 replies
  • 0 kudos

Major Bug when erasing a projet

how to reproduce:Create a new projet with a "namePrj" and "directory". The normal way should be to have a directory "directory"/"namePrj", and in this directory, all the project files (like with STM32CubeMX). But the files a created in the "directory...

ANauz.1 by Senior II
  • 5021 Views
  • 11 replies
  • 2 kudos

ST-Link upgrade error on Nucleo F446RE

I run CubeIDE on Linux and when I want to Debug, it prompts for an ST-link upgrade. I click Yes and I get screenshot no. 1. The ST-LINK ID displayed there is correct, I get the same ID with "st-info --probe".Then I click on Open in update mode, and I...

aro by Associate III
  • 6975 Views
  • 9 replies
  • 0 kudos

Why is STMcubeIDE not detecting my device?

Hi all, I am trying to run a program from STM32cubeIDE to my STEVAL-MKI109V3 board, however the IDE is not recognizing my board. The device is listed in Device Manager under Ports&COMs as "STMicroelectronics Virtual COM Port (COM5)" so this leads me ...

ZoeTakacs by Associate II
  • 1571 Views
  • 1 replies
  • 1 kudos

stm32cube to compile legacy arm syntax?

Hi folks,I have an assembly file with 2.5k lines and I'm facing a compiling issue.It seems that the problem is about the syntax -GNU compilation support a specific syntax while arm leagacy syntax is different. In example:name EQU 0xC vs.equ name 0xC ...

kingkong by Associate
  • 1894 Views
  • 2 replies
  • 0 kudos

[STM32WL55] Boot in low power mode.

Hello everyone!I'm wondering about a possible solution for our device working on a STM32WL55.For hardware reasons, it would be nice to boot the device directly in low power mode (possibly STOP2).I can't seem to find any answer to this question online...

LorenzoC by Associate
  • 940 Views
  • 0 replies
  • 0 kudos

Resolved! SPI COMMUNICATION THREE WIRE/ FOUR WIRE

Hi,I have doubt with the spi communication setup in this configuration. I'm using two sensors where one of the sensor only support 3 wire spi and another  is 4 wire .I have a single spi in mcu. The hardware setup is followed by mapping four wire spi ...

Resolved! How to use the SWV statistical profiling menu in stm32cubeide.

I am developing a device using stm32f429zit6. I want to know the usage rate of all software functions in the project, how to use the SWV statistical profiling menu in stm32cubeide? After setting Debug (Trace Asynchronous Sw), debugger menu, and seria...

image1.png image2.png image3.png image4.png
joseph05 by Associate III
  • 3367 Views
  • 1 replies
  • 0 kudos