STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1554 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 588 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

Resolved! UART not working as expected

Hi,When I run the below code, I get the result on serial console as in below image which is not as expected. Could you please let me know what I am missing here ?   int main(void) { /* USER CODE BEGIN 1 */ DWT->CTRL |=(1<<0); /* USER CODE END ...

demir_1-1709326501923.png demir_0-1709325904032.png
demir by Senior II
  • 2949 Views
  • 4 replies
  • 3 kudos

STM32CubeIDE opens on non-present screen.

Win 11 Laptop with external (large) monitor.When the laptop is then used without the external monitor, apps should open on the internal one.Most do; STM32CubeIDE (v1.13.0) doesn't - it still positions itself as it the non-connected screen were still ...

AndrewNeil_0-1709311291831.png

Resolved! Debugger hangs when starting a timer with interrupt

I'm using an STM32F446RE MCU on a custom board and I developed a custom bootloader. The bootloader starts at 0x8000000, while the application code starts at 0x8008000. Inside the bootloader I use timer 14 with interrupt and when I need to jump I use ...

DamianoF by Associate III
  • 2248 Views
  • 1 replies
  • 0 kudos

Error when debugging with assembly window offset -> length

 Hello,In the past 2 days, I have an errorwhen I launch the debugger and it looks the issue comes from eclipse. When I launched the debuger, I have this error window.I uninstalled CubeIDE, and installed it again (tried 3 different versions).I can dow...

JMene1_0-1707483960301.png JMene1_0-1707484097056.png
JMene.1 by Associate III
  • 1974 Views
  • 2 replies
  • 0 kudos

Resolved! GPIO initialization for STM32F769I-DISCO

Hello,I want to do GPIO initialization for STM32F769I-DISCOhere, i am using those pins in my code: {GPIO_InitStruct.Pin = EV2_Pin|AF1_Pin|WF5_Pin; GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_PP; GPIO_InitStruct.Pull = GPIO_NOPULL; GPIO_InitStruct.Sp...

Dynamic memory allocation problem

HiI have a weird problem and do not understand where it could come from and thus do not know how to solve it. I am adding list entries to a list, and it seems to function correctly when I add them hardcoded. However, when attempting to add an entry r...

MFäh.1 by Associate II
  • 1822 Views
  • 2 replies
  • 0 kudos

stm32 with stepper motor driver tmc2660

Hi ,in my project i was having a requirement  that the three stepper motors are need to work using STM32 -> TMC429 motion controller -> TMC2660.THE SPI communication between the TMC429 and MICROCONTROLLER is working, and verified. but in the case of ...