STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1420 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 558 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

Resolved! Cant do anything with the board

I'm a new user working with a Nucleo F103RB board, and it suddenly stopped working. I can't program, debug, perform a chip erase, or access any sector. It began showing vFlash errors and is now stuck in a lockup stage. I've attempted to upload a diff...

Captura de tela 2024-05-13 143641.png

Resolved! J-link driver manual upgrade for STM32U5G9J-DK1.

Hello,  I tried to use a J-Trace to program an STM32U5G9J-DK1.  This J-Trace Pro works well on other projects.  I also tried a J-link and it shows the same issue. While, of course, STLink3 via the same connector works well.  After I look into the J-l...

lhz412 by Associate II
  • 3436 Views
  • 1 replies
  • 0 kudos

STM32CubeIDE 1.15.0 released

STM32CubeIDE 1.15.0 was released today on st.com as well as an in-tool update patch. What is new in 1.15.0? Microcontroller and board lists aligned with STM32CubeMX v6.11.0 : STM32U0, STM32H7Rx/STM32H7Sx and STM32H523/STM32H533Added the support for t...

STM32 CUBE IDE - taskEntry() function definition

Hi team,I am developing a POC to change screen when we click an icon on the display in STM32 Cube IDE. I am using STM32F429I Disco board with ili9488 LCD driver and tsc2004 Touch Sensor Controller. I have developed the Graphics in TouchGFX designer. ...

Resolved! STM32CubeIDE 1.15.1 code generation problem

Using TIMER4 - CH1 as PWM generator with DMA1 - Channel1 (memory to peripheral, circular mode, Half Word), the code generation produces this output in file tim.c:                where (see red arrow) it uses DMA_REQUEST_TIM1_CH1 instead of DMA_REQUES...

Test01.jpg