Skip to main content
Visitor II
September 26, 2024
Solved

STM32IDE Login problem

  • September 26, 2024
  • 1 reply
  • 1553 views

Hello, I'm having an issue with my STM32IDE. I just installed it, and when I try to log in, I press the "myST" -> "Login" button, and it opens a box called "User Authentication Dialog," but it's blank, and I can't log in. This is important because many features require logging into the IDE, and I can't work properly without it. 

Daniberos_0-1727389645167.png

 

This topic has been closed for replies.
Best answer by Semer CHERNI

Hello @Daniberos 

First let me thank you for posting.

Let's start by checking your network parameters.
Are you using any proxy to connect? If it's the case check this article on how to configure the network settings for STM32CubeIDE and STM32CubeMX : How to set the network connection parameters for S... - STMicroelectronics Community

Also the article describe how you can install FW packs manually without connecting.

KR,
Semer.

1 reply

Semer CHERNI
Semer CHERNIBest answer
ST Employee
September 27, 2024

Hello @Daniberos 

First let me thank you for posting.

Let's start by checking your network parameters.
Are you using any proxy to connect? If it's the case check this article on how to configure the network settings for STM32CubeIDE and STM32CubeMX : How to set the network connection parameters for S... - STMicroelectronics Community

Also the article describe how you can install FW packs manually without connecting.

KR,
Semer.

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.