STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1433 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 560 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

Failed to start GBD server. No device found on target.

I designed and printed two PCBs featuring the STM32H743 microcontroller. I initially worked with the first PCB without any issues, but it suddenly stopped functioning, and the chip was no longer recognized. After numerous unsuccessful attempts to res...

Juanlu by Associate
  • 1334 Views
  • 1 replies
  • 0 kudos

STM32CubeIDE for Apple Silicon

I am installing the STM32CubeIDE on a new Apple Silicon laptop, but apparently the packaged version is for Intel CPUs, because upon install the OS requires to install Rosetta. Will it be available in future a version of STM32CubeIDE (and of STLink Se...

PB1 by Associate III
  • 2559 Views
  • 2 replies
  • 2 kudos

Bug #2 in X-CUBE-AZRTOS-H7 V3.3.0

Hello STM-Guys,There's a bug in X-CUBE-AZRTOS-H7 V3.3.0, which affects the memory assignment.I declared the following memory assignment:This generates the attached "STM32H723ZGTX_FLASH.rar" file. The memory declarations are in the file, but those are...

Intector_0-1733100507194.png

Resolved! STM32L496G-Disco Pin Configuration question

Hello,I am new to stm programming. I got a STM32L496G-DISCO board and I wanted to create a new project. When I try to configure the pins i have a lot of yellow triangle warning icons and some of the fields are purple which can not be changed. I don't...

AndreeaP31_0-1732472011140.png AndreeaP31_1-1732472076599.png

H7 QSPI XIP single mode demo fails

Hello,I succeed to run all demo programs of the H7 performance suite (STM32CubeExpansion_Performance_H7_V1.0.0) except the QSPI single mode demo (8 - D1_QuadSPI_Single - D1_DTCM) on STM32H753I_EVAL2. But I can run the dual mode demo (9 - D1_QuadSPI_D...

function_call.png wrong_code.png signal_handler.png
regjoe by Senior II
  • 3711 Views
  • 8 replies
  • 1 kudos

SBSFU_Boot on STM32H743

Hi there.I downloaded the SBSFU_Boot project from the examples in STM32CubeIDE.The SBSFU_Boot project is designed for STM32L552ZET6QU.I am considering applying SBSFU_Boot to STM32H743.Could you please explain in detail how I can apply it?It would be ...

Resolved! GitHub actions integration

Hi,I'm looking into utilizing GitHub actions for CI/CD. I couldn't find any examples of how to use GitHub actions to build a STM32CubeIDE project automatically. Any hints/directions?Thanks,

YKuo.1 by Associate II
  • 7394 Views
  • 8 replies
  • 5 kudos

Resolved! STME32CubeIDE + FreeRTOS - file "freertos_mpool.h" missing

Hello, I am using STM32CubeIDE to compile under FreeRTOS a project to download in an ARM STM32F107VCT6 component installed on an Olimex board.I am new to using STM32CubeIDE.At first, I just want to run a very small program on the component to make a ...

MDe by Associate III
  • 4882 Views
  • 2 replies
  • 0 kudos