STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1440 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 562 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

Resolved! Capturing SWV data stream from GDB

I've got SWV output showing within the STM32CubeIDE. I would now like to be able to capture this output from the command line using gdb. Is there any documentation on how to activate the SWV in gdb?I've tried using: monitor swo enable 4500000 decode ...

CTapp.1 by Senior III
  • 1127 Views
  • 1 replies
  • 0 kudos

Resolved! Graphics change on the display through the code

Hello guys can someone please help me change the graphic on the display through the code? My boss sent me a video in French, which I don't understand at all. I've already Googled and searched but haven't found anything yet. I'm using the STM32746G-Di...

Bea_12 by Associate III
  • 1121 Views
  • 2 replies
  • 2 kudos

Disable Helium extension using STM32 cube ide

Hi all,I am using the STM32N6570-DK kit with the GCC compiler. I want to disable the Helium extension. I have taken the AI object_detection code as a base code and created one function to check whether the Helium extension is enabled or disabled. I r...

VasuV by Associate II
  • 2128 Views
  • 3 replies
  • 0 kudos

CMSIS DSP 1.16.2 || NUCLEO-H7S3L8 || H7S3L8

STM32Cube IDE Version: 1.17.0  CMSIS-DSP 1.16.2 NUCLEO- H7S3L8Below  a suggested solution for those using CMSIS-DSP 1.16.2 together with NUCLEO-H7S3L8 (this may be generalized to other similar configurations) as I 've been myslef browsing a couple of...

AudioDev by Associate II
  • 1288 Views
  • 1 replies
  • 0 kudos

Resolved! Firewall blocking ST Login?

I can't login into ST to download packages via CubeMX/CubeIDE. The wheel turns forever, no matter what proxy settings I choose. The pack downloader works - I just can't log into ST which is a pitty.Which url does my corporate IT whitelist?See similar...

JKapp.1 by Associate III
  • 1337 Views
  • 4 replies
  • 0 kudos