STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1440 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 565 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

Cube_IDE color

Hello, Is it possible to change the color of the tabs on Cube IDE? See attachment.Best regards.Sebastien. 

PSEBA.1 by Associate II
  • 836 Views
  • 1 replies
  • 0 kudos

Resolved! STM Cube IDE installation problem in RHEL

I am facing an issue while installing the cube ide in  my rhel 9.2 version,the exact problem was when i try to run the executable file and going through the instructions ,after agreeing the licenses and the folder which contains .rpm files is deletin...

undefined reference to `SEGGER_RTT_ASM_WriteSkipNoLock'

Hi,i am trying to port FreeRTOS to my STM32L152RCT6.i did it successfully.but when i am trying use segger debug tool.i am facing issue like this  18:09:25 **** Incremental Build of configuration Debug for project freertosporting **** make -j4 all ar...

chaithu by Associate II
  • 2856 Views
  • 4 replies
  • 0 kudos

STM32CUBEIDE inc src hidden

I wanted to check out the HID Master USB example from ST for my STM32H7B3I-DKIt would not compile, forcing me to upgrade my CubeIDENow it compiles, but inc & src folders do not appear in Project explorer.  They are there on the hard diskThe inc and s...

BBrow.2 by Associate III
  • 1233 Views
  • 2 replies
  • 0 kudos

Resolved! How can I add files to a STM32CubeIDE project as links?

If anyone is familiar with Code Composer IDE, CCS allows me to add files to a project as links. If this is not possible, perhaps you might have suggestions of how to share common code files between projects without replicating the common code.

phgphd by Associate II
  • 6084 Views
  • 5 replies
  • 0 kudos

Issue in creating new project using STM32IDE

Hi team,I am using STM32IDE version 1.7.0. when I trying to create new project by selecting STM32F373VC as the controller. I am getting an error message saying, "Error downloading the following files: stm32cube_fw_f3_v1115.zip (Timeout during downloa...

KKB by Associate
  • 1741 Views
  • 1 replies
  • 1 kudos