STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1440 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 561 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

Resolved! Include paths (-I) stopped working

Hi all, Previously, I've been adding all paths with the used header files in the Project->Properties->C/C++ Build->Settings->MCU GCC Compiler->Include paths->Include paths (-I), like this:It has been working pretty well, until it just stopped. The la...

pav_ivanovs_0-1742989958331.png pav_ivanovs_1-1742990203356.png

Debug launch appears to end up in bootloader

I have a NUCLEO-L4R5ZI board with an STM32L4R5ZIT6P MCU. I have been successfully building and debugging using CubeIDE 1.9.0 with a USB connection to the onboard ST -LINK debugger. However, I've suddenly encountered a situation where after the debug ...

Resolved! Enable SWO on CubeIDE 1.12.1 - Board used Nucleo-H755ZI

Hello,I went through all the SWO related topics, and it was a bit confusing for me to get it running, so I summarized the steps to have it working on a Nucleo H755.In my project I have the main clock set at 400MHz, Timer2 running at 1Hz and Debug set...

MD_1-1687436178095.png MD_5-1687437990558.png MD_2-1687436299945.png MD_3-1687437584204.png
MD by Associate II
  • 5145 Views
  • 4 replies
  • 0 kudos

Getting started with STM32 - Basic questions2

Hello Experts,I have brought the STM32F407G-DISC1 discovery board and have a few more basic questions.1.What is the correct way to select the RAM or FLASH configuration? As of now the way i do this is :"project properties -> C/C++ Build -> Settings -...

ak52_1-1742906717896.png ak52_0-1742906462056.png ak52_0-1742912889791.png
ak52 by Associate III
  • 1262 Views
  • 1 replies
  • 0 kudos

No ST-LINK detected Error message

I have been running an STM project for the past month using a NUCLEO STM32F401RE. Almost every time I try to run the program for the first time that day, I get an error message that there is no ST-LINK detected. Sometimes it will connect after a whil...

atzi by Associate
  • 1779 Views
  • 2 replies
  • 1 kudos

Resolved! St-Link is not detected MacOS 15.3.1

Hello,I update my computer to MacOs 15.3.1 and I have a similar problem to when MacOs 15 arrived. The St-Link (ST-Link v3 mini) is not detected with Cube IDE (CubeIDE v. 1.17.0).It worked fine in MacOS 15.1.1I've tried starting the IDE as admin and a...

MA4 by Senior
  • 3905 Views
  • 6 replies
  • 0 kudos

slow data dump from Memory Browser window

Hello,I need to download some floating point arrays from STM32CubeIDE (v1.17.0).  As understood, the only way to do this is to bring the array up in a Memory Browser window, and then select Export, to a file.  Since this is in byte format, I then pos...

R_DSP by Associate II
  • 663 Views
  • 0 replies
  • 0 kudos