User Activity

Hello,I update my computer to MacOs 15.3.1 and I have a similar problem to when MacOs 15 arrived. The St-Link (ST-Link v3 mini) is not detected with Cube IDE (CubeIDE v. 1.17.0).It worked fine in MacOS 15.1.1I've tried starting the IDE as admin and a...
Hello everyone,I program on stm32h757 with stm32cube IDE on macOS Sonoma. (stlink v3 minie)Until recently, I debugged with the st link and displayed printf in the swv console without any problem.For technical reasons, I made the program work with the...
Hello, I am working on a project with a dual core processor (H7) and I have some display problems in my IDE (STM32CubeIDE v1.9.0). For example, I added the LWIP part to my board with #define LWIP_IPV4 1 and #define LWIP_DHCP 1.When I am in debug mode...
Kudos from
Kudos given to