STM32CubeIDE (MCUs)

Ask questions on STM32CubeIDE. Discuss how to build, debug, configure, and optimize your project as well as how to use our software tools.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeIDE 2.1.1 released

We are pleased to announce that the minor version 2.1.1 of STM32CubeIDE is available. What is new in 2.1.1: This release covers the topics listed below: SEGGER J-Link GDB server updated to 9.24 to fix an issue with the Live Expression view during the...

Aimen1 by ST Employee
  • 1436 Views
  • 0 replies
  • 1 kudos

STM32CubeCLT 1.21.0 released

We are pleased to announce that STM32CubeCLT 1.21.0 release is available. What is new in 1.21.0: Maintenance of the previous version: Updated in accordance with STM32CubeIDE v2.1.0Update of Clang/LLVM toolchainUpdate of GCC to GCC 14Update of STM32Cu...

Aimen1 by ST Employee
  • 560 Views
  • 0 replies
  • 0 kudos

STM32CubeIDE 2.0 release - early heads-up!

Starting from the release in November 2025, STM32CubeIDE and STM32CubeMX will be available exclusively in their standalone versions. STM32CubeMX will no longer be integrated inside STM32CubeIDE. Instead, the two tools will be interoperable in the sam...

Resolved! Does SWV work on the STM32H573 DK board?

Beside enabled it in the Debugger tab:also called LL_DBGMCU_EnableTraceClock();but when calling ITM_SendChar(), the ITM->TCR is still 0.Do I miss anything else?  BTW, I am using the latest STM32CubeIDE 1.18. Thanks.

Thatseasy_0-1743125055947.png
Thatseasy by Associate III
  • 843 Views
  • 1 replies
  • 0 kudos

stlink_gdbserver gdb-multiarch

I'm trying to debug some embedded rust. I was using openocd (12) and gdb-multiarch. I currently using an stm32f3discovery. I've tried C with eclipse Embedded ARM and STM32CubeIDE and while STM32CubeIDE does work (validating my hardware) nothing else ...

beattie by Associate II
  • 2565 Views
  • 5 replies
  • 0 kudos

Resolved! Error when debugging: Failed to execute MI command

I have a project that ran without issue, with STM32CubeIDE 1.13.0. When I updated it to 1.17.0 I could no longer debug that same project. The error window says:Error in final launch sequence: Failed to execute MI command:load D:\\Proyectos\\STM32Cube...

MRey.1 by Associate III
  • 3499 Views
  • 6 replies
  • 1 kudos

Changing on Display

Hello everyone,I am currently working with the STM32F746 and have implemented a brightness controller. I can control the regulator via code (CubeIDE) and assign a value. However, I don't understand how to make the display actually adjust its brightne...

Bea_12 by Associate III
  • 760 Views
  • 1 replies
  • 0 kudos

STM32CubeIDE 1.5.0 released

STM32CubeIDE 1.5.0 released STM32CubeIDE 1.5.0 was released this week on st.com as well as a in-tool update patch. Caution: The in-tool update does not allow updating drivers and ST-LINK server tool. Full installer is required for this.What is new in...

Resolved! Override Breakpoint at 'main' ?

 Is there a way to have this breakpoint only enabled at the start of the debug session?So, when the code is first loaded, it will stop at main(); but then after subsequent resets I set my own breakpoint.It doesn't appear in the list of breakpoints, s...

AndrewNeil_1-1743163673370.png

Resolved! Oscillators with STM32C071RBT6

Hello to everyoneI'm using the board NUCLEO-C071RB. I already done the firmware, and it seems work fine.Because now i must build my board i check again my project:I forgot to set PF0-PF1 (Osci IN OUT) and PC14-PC15(OSCX IN OUT). It would huge problem...

gbgbytybhome.png freferme.png