STM32 MCUs Wireless

Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NUCLEO-WBA25CE1 "Bootloader limitation"

Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.

ctrois by ST Employee
  • 240 Views
  • 1 replies
  • 1 kudos

Matter software expansion for STM32Cube

Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link  MATTER - Matter software expansion for STM32Cube - STMicroelectronics  It is a reference implementation for the demonstration of Matter on ST...

Ouadi by ST Employee
  • 4082 Views
  • 0 replies
  • 3 kudos

Resolved! STM32WB15 Error: FUS_STATE_ERR_UNKNOWN: Unknown error

Hi,I'm faced to a problem and i'm no more able using the FUS in order to update the BLE STACK: i get this error message: "FUS_STATE_ERR_UNKNOWN: Unknown error when i clicked on the START FUS button on the STM32CubeProgrammer tools (V2.13.0)we tried t...

Resolved! STM32F429IGT6 Dual Bank OTA updates

Hi folks,I am trying to implement a dual bank OTA system on my STM32F429IGT6 using DBM1 and BFB2 in the STMCubeProgrammer, but I'm having trouble booting into the second flash region (which I will call app_b from now on, along with app_a for the firs...

Resolved! Nucleo-WL55JC as gateway

Hello, I'm using Nucleo-WL55JC cards and I wanted to know if it was possible to use them as gateways, partly to connect the radio world to the internet (LoRaWAN), and partly to extend the range of my network (by dispersing multiple gateways everywher...

KYZ by Associate III
  • 4160 Views
  • 14 replies
  • 4 kudos

STM32Wl55CC connection error for SWD programming

I am trying to make a prototype from a perf-board and a QFN48 adapter using STM32WL55CC MCU based on the wiring in the pics below.  I want to connect to the MCU using SWD via an STlink attached to a Nucleo board. I already removed the 2 jumpers on CN...

STM32WB55CG Zigbee

Hi, I have a project which uses P-NUCLEO-WB55 as reference design. However, I'm facing some problems after the customization has done on the USB Dongle demo board. Below is the problem scenario.1. After configured M4 CPU to USB HID class eg. Keyboard...

Phang by Associate III
  • 1132 Views
  • 5 replies
  • 0 kudos

ST-ICUBE-LRWAN - What's the planned development?

Dear ST and Community,We are using STM32L series in a variety of LoRaWAN IoT Devices.We have 10 products and have produced roughly 0.5M units so far.We use the I-CUBE-LRWAN project for a long time. It's a great project, but it looks like the developm...

lyanchev by Associate
  • 1310 Views
  • 1 replies
  • 0 kudos