User Activity

Hi, I am building a BLE application using Zephyr v3.7.0 and nucleo_wba55cg evaluation board. I have currently implemented the accept list functionality where only paired and bonded devices can connect in accept list adv mode. However, I struggle with...
Hi,I am currently using Zephyr v3.7.0 to program the Nucleo STM32WBA55CG board running BLE peripheral based application.Since our project has flash and RAM constraints, I would like to explore the peripheral only BLE library to reduce the  memory foo...
Hi, I am programming the STM32 NUCLEOWBA55CG with Zephyr v4.0.0 and our application is using the BLE stack.Due to flash limitations, we would like to use the basic stack and link layer BLE libraries for the STM32WBA series  (see communication with ST...
Hi,I am programming the nucleo_wba55cg using Zephyr v3.7.0.My application is based on a BLE peripheral example, whereby I have also configured an LED on the nucleo_wba55cg board to toggles at the rate of 1s.Also, I modified the rcc section the nucleo...
Hi, I am using the STM32 Nucleo WBA52CG evaluation board and programming it using Zephyr v3.7.0 and am looking how to set the Tx output power of the BLE radio. Are there any configs available in Zephyr for the same?  If not, alternatively please sugg...