cancel
Showing results for 
Search instead for 
Did you mean: 

Enabling FREERTOS deletes my STM32_WPAN BLE settings in STM32Cube_FW_WB_V1.8.0

BPaik
Senior

I have a project using the STM32_WB55 where I use CubeMX to setup a custom BLE template, services, characteristics, etc. I noticed that STM32Cube_FW_WB_V1.8.0 supports both BLE and FREERTOS, but when I enable FREERTOS, all my custom BLE settings are deleted. Additionally, many of the configuration tabs appear to be missing. I see there is an option to setup the heart rate sensor, but adapting this to match my initial custom BLE configuration seems to be a lot of effort compared to generating a custom template. Is there a way to use my custom template with FREERTOS in CubeMX? If not, is this something that will be supported in a future version?

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
Remi QUINTIN
ST Employee

​In fact only the Hearth Rate profile is supported with FreeRTOS in CubeMX. Hence the strange artefact you got with your BLE settings.

Will support for custom BLE templates with FreeRTOS be added in a future release of CubeMX?