STM32 MCUs Wireless

Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NUCLEO-WBA25CE1 "Bootloader limitation"

Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.

ctrois by ST Employee
  • 221 Views
  • 1 replies
  • 1 kudos

Matter software expansion for STM32Cube

Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link  MATTER - Matter software expansion for STM32Cube - STMicroelectronics  It is a reference implementation for the demonstration of Matter on ST...

Ouadi by ST Employee
  • 4067 Views
  • 0 replies
  • 3 kudos

Resolved! STM32CubeMx generating sources with errors

I am trying to initiate a project via cubeMx for the STM32WB55 nucleo board.I an able to initiate a simple project without the BLE middleware (STM32_WPAN).Once adding the STM32_WPAN, the generated project not compiled on both Atollic true studio and ...

~Amit~ by Associate III
  • 4268 Views
  • 9 replies
  • 0 kudos

Error upgrading wireless coprocessor firmware on Nucleo-68

I am experiencing an error while trying to upgrade a Nucleo-68 board from P-NUCLEO-WB55 wireless coprocessor to latest v1.7.0 firmware provided by STMicroelectronics/STM32CubeWB github repo.I already reported the issue on the githb repo here is a cop...

anddam by Associate II
  • 4217 Views
  • 17 replies
  • 0 kudos

Custom STM32WB55CC board - unable to upgrade FUS

Hi,I am developing an application for custom built STM32WB55CC board. Everything seems to be fine, however I am not able to upgrade FUS from v0.5.3. I am reproducing steps from release notes attached inside 1.8.0 FW pack. Please find a log from delet...

bnowicki by Associate
  • 701 Views
  • 0 replies
  • 0 kudos

STM32CubeWL MCU package

Hello ST Team, I would like to use the STM32WL in a project that ends at the end of the year.When can I expect the STM32CubeWL MCU package to be released (Q4 was mentioned in a post -> Too rough)?Would it be possible to get a preliminary (also untest...

CHe by Associate II
  • 1236 Views
  • 2 replies
  • 0 kudos

CMSIS OS2 Wrapper and Software Timers

Dear ST,   the current version of the CMSIS OS2 wrapper (V1.8.0 for STM32WB) does not support calling the functions osTimerStart() and osTimerStop() from an ISR. However, FreeRTOS does provided the functions xTimerChangePeriodFromISR(), xTimerStopFro...

roman1 by Associate III
  • 4234 Views
  • 5 replies
  • 0 kudos

Resolved! Other suppliers for components in reference design ?

For an R&D project we are curently designing a PCB around an stm32WB , we use the stm32W55 usb dongle as reference design for our project.But we are currently not able to source some specific components : L3 : Ferrite FCM1608KF-601T0FLT1 : band pas...

PJEAN.1 by Associate II
  • 1544 Views
  • 2 replies
  • 0 kudos

USB_CDC and BLE Hard Fault

Hello,I'm using CubeMx to create a project with usb cdc serial port and BLE functionality. CubeMx generates a sequencer UTIL_SEQ_Run(~0); that runs the BLE state machine. In the code below, if I comment out UTIL_SEQ_Run(~0); the code runs fine per Wo...

0693W000003C5bNQAS.png
BMart.2 by Associate II
  • 2794 Views
  • 5 replies
  • 0 kudos