STM32 MCUs Wireless

Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NUCLEO-WBA25CE1 "Bootloader limitation"

Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.

ctrois by ST Employee
  • 220 Views
  • 1 replies
  • 1 kudos

Matter software expansion for STM32Cube

Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link  MATTER - Matter software expansion for STM32Cube - STMicroelectronics  It is a reference implementation for the demonstration of Matter on ST...

Ouadi by ST Employee
  • 4065 Views
  • 0 replies
  • 3 kudos

Resolved! BLE: detect security level

Hi,i have 2 boards (client and server) with STM32WB that communicates through BLE messages. Right now, at every reboot/disconnection i am redoing the pairing, but it is really slow.In order to reduce the whole connection time, i am trying to use the ...

LSpad.1 by Associate III
  • 1796 Views
  • 1 replies
  • 0 kudos

Does SRAM2 parity work with the BLE stack?

Greetings,My application for the STM32WB uses the BLE full stack from v1.8 of the Cube. I just noticed that there is a v1.10. I plan to test this as well, just in case this has been fixed.The cube has code to manipulate the SRAM2 parity options, but ...

eleventen by Associate III
  • 828 Views
  • 0 replies
  • 0 kudos

Why device using I-Cube-LRWAN software send random data when uplink_counter reach 65535 sent ? Is there any way to modify it ?

Hello Everyone, I'm working with the I-Cube-LRWAN software for LoRa communication in class A device.The device sends data every Tx_Dutycyle period but I have an issue with the software.When using the stack connected to Network such as TTN, I notice t...

How to turn off MAC debugging information in STM32WB

Hello, I am using the STM32WB-P-NUCLEO-WB55 board to do a thread experiment. When I use the serial port assistant to read the messages, I found that many messages that are not on the application layer are displayed.For example, the displayed MAC laye...

0693W000006EHLmQAO.jpg
ZB.1 by Associate II
  • 761 Views
  • 0 replies
  • 0 kudos

Resolved! VBAT Channel Monitoring in the MCU

Datasheet of STM32WB55 mentions that the Maximum voltage that can be given to VBAT is 3.6 V. But, it is also said that there is an internal voltage divider so that voltage to the ADC is 1/3 of the voltage at the VBAT pin So, is it possible to connec...

ASiva.1 by Associate III
  • 3509 Views
  • 3 replies
  • 0 kudos

Resolved! Zigbee stack for STM32WB30 with CubeMX

Hi,I'm looking to create an zigbee endpoint device. I've selected the STM32WB30 for my project and have been configuring in CubeMX. This all goes well.Now I need to flash an wireless stack to the M0, but there is no zigbee stack for the STM32WB30.Doe...