STM32 MCUs Wireless

Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NUCLEO-WBA25CE1 "Bootloader limitation"

Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.

ctrois by ST Employee
  • 221 Views
  • 1 replies
  • 1 kudos

Matter software expansion for STM32Cube

Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link  MATTER - Matter software expansion for STM32Cube - STMicroelectronics  It is a reference implementation for the demonstration of Matter on ST...

Ouadi by ST Employee
  • 4066 Views
  • 0 replies
  • 3 kudos

With the "STM32 LoRa® Expansion Package" is it possible to set the RTC time after initialization of the Lora stack.

I would like to be able to set the time from the LoRa network. So when I receive the time I make a HAL_RTC_SetTime with the information collected, but then my program freezes. Do I have to stop the Lora layer, timers beforehand?Thank you in advance f...

LeJiBXL by Associate
  • 1164 Views
  • 1 replies
  • 0 kudos

STM32WB USB bootloader

HiI`m having some issues with programming p-nucleo usb dongle board with USB DFu mode.The way I understand is ,there is an internal system bootloader inside STM32WB which supports USB Firmware DownloadIf I can jump to bootloader from my application ...

TGUCL.1 by Associate III
  • 982 Views
  • 0 replies
  • 0 kudos

CMWX1ZZABZ-091 -StandBy/Stop mode and Power consumption.

Dear Members. I'm a beginner and trying to learn and understand how to work with stm32l0 and SH1276. The first task which i set to myself is to reach the absolut minimum power consumption. Watched some tutorials and tried to reach minimum which i me...

GWisn.1 by Associate
  • 1431 Views
  • 2 replies
  • 0 kudos

I-CUBE-LRWAN don't work on custom board: PHY txTimeOut ERROR

Helloi made a customised board using the STM32L476RETx mcu with a lora module : DORJI DRF1262TI opened the project from i-cube-lrwan expansion package with the name SX1262dvk1das USING THE SX1262 AT 868MHz.i updated the PINOUT of my MCU and exclude a...

SHATE.1 by Associate III
  • 1518 Views
  • 1 replies
  • 0 kudos

Resolved! UART example for STM32WB55 "printf" prints gibberish. I see, the characters are sent to "HAL_UART_Transmit" are correct. BLE HRT example prints debug messages correct.

The printed message is:▒▒RT ▒▒▒n▒▒ E▒amp▒▒ ▒▒▒a▒g▒▒ ▒h▒ C ▒▒b▒a▒y p▒▒n▒▒ ▒un▒▒▒▒n ▒▒ ▒h▒ ▒▒RT▒Insteadprintf("UART Printf Example: retarget the C library printf function to the UART\n\r");

VadymS by Associate II
  • 2641 Views
  • 3 replies
  • 0 kudos