STM32 MCUs Wireless

Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NUCLEO-WBA25CE1 "Bootloader limitation"

Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.

ctrois by ST Employee
  • 219 Views
  • 1 replies
  • 1 kudos

Matter software expansion for STM32Cube

Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link  MATTER - Matter software expansion for STM32Cube - STMicroelectronics  It is a reference implementation for the demonstration of Matter on ST...

Ouadi by ST Employee
  • 4065 Views
  • 0 replies
  • 3 kudos

Resolved! Where is the documentation on the Sequencer?

Looks like the Scheduler, SCH_*, have been replaced by the Sequencer, UTIL_SEQ_*. Does anyone know where there is detail description of the Sequencer, along with examples?Thanks,Mark

NPham.11 by Associate
  • 2234 Views
  • 2 replies
  • 0 kudos

STM32WB55 sometimes hangs during BLE Init

I am using the Nucleo STM32WB55 Nucleo Pack to develop BLE applications on the Nucleo board. Every once in a while I have the problem, that the application does not properly start and hangs during BLE Init of the co-processor. This is no problem of m...

MDaub.1 by Associate III
  • 1807 Views
  • 1 replies
  • 0 kudos

no send with the module lora b-l072z-lrwan

hello,I use the B-L072Z-LRWAN Module in Lora, i want test the AT CommandI Join the module AT+JOINAT+NJS=? ==> 0I send AT+SEND=12:hello the response:AT_ERRORI don't understand why?best regardMichel

MArna.19 by Associate
  • 764 Views
  • 0 replies
  • 0 kudos

Resolved! have a problem on linker

I built the project using the STM32CubeExpansion_LRWAN_V1.1.2 example, and I want to use the EEPROM function in LoRa Application.I am trying to declare eeprom related code in a separate file, but the linker cannot import HAL functions.​.\mlm32l07x01\...

DPark.2 by Associate II
  • 3252 Views
  • 6 replies
  • 0 kudos

HELP - CMWX1ZZABZ-078 project on STM32CubeIDE

Hello everyone, I'm trying to compile together a project Created with STM32CubeIDE based on STM32L082 and STM32CubeExpansion_LRWAN_V1.3.1 but I'd like to keep it configurable through CubeMX.Is there someone that succeded in this? There are a lot of f...

AComa.170 by Associate II
  • 1845 Views
  • 2 replies
  • 0 kudos

I'm trying to implement custom callbacks on the STM32WB Zigbee library. Any examples of custom callbacks on a report or certain attributes?

My goal is to have a coordinator connected to sleepy end devices. The coordinator will periodically request measurements from the end devices. It seems like all the examples have requests going from the nodes to the coordinator, so I'm having trouble...

MCope.1 by Associate II
  • 2773 Views
  • 4 replies
  • 0 kudos

Resolved! STM32WB55 : Using event process functions tables.

Hi.In SDK I foud interesting source files: ble_events.h, ble_events.c, in wich we have 3 structures defined as hci_event_table_t.Also in ble_legacy.h we have a defines to that structures.Every strucrure have event code and callback and callback calls...