NUCLEO-WBA25CE1 "Bootloader limitation"
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link MATTER - Matter software expansion for STM32Cube - STMicroelectronics It is a reference implementation for the demonstration of Matter on ST...
Please go and visit our wiki pages where you can find a lot of information on our wireless product families (WB, WBA, WL) and the supported protocols: BLE, Zigbee, Thread, Matter, Lora, ... To begin your technical journey, please start from this top ...
Hello! At first I want to apologize for my bad english.I faced with the following problem.I have device with STM32L476 MC and STM32WB55CE. Input voltage around 4 V. This voltage go the the switching voltage regulator TPS63050RMWT. After switching on ...
Hi, i watched the video (https://www.youtube.com/watch?v=WgsXMVZfoO8) from the getting started series. I followed the steps and everything worked til running the example. If I press debug everything starts and the led 6 blinks red and green. The cons...
I'm trying to get the idle power consumption of down to a few uA, but I cannot get it lower than around 920uA which is all being consumed by I_SYS.Has anyone been able to get it lower?I'm using the DCDC and TCXO (as far as I know).I don't think it wo...
Hello guys,I am using STM32WB and also get stuck when I try to enable hci_le_advertising_report_event()I use examble BLE_MeshLightingRFL and in function Ble_Hci_Gap_Gatt_Init(), I command function aci_gap_create_connection() at the endIt return BLE_S...
Hello?Likes title, I want to ask for writing method using ST-Link(SWD, 4000 kHz).Problem is error at erasing stage. "Error : FUS_STATE_ERR_UNKNOWN"(Version of STM32CubeProgrammer is 2.5.0, result of this UI also same.)And, result of reading addre...
I am using STM32L152RET6 running I-CUBE-LRWAN V1.2.1 CLASS A. I am pushing data to TTN and I can perfectly see the uplinks and downlinks from my LoRaWAN Gateway (RHF0M301):JSON up: {"rxpk":[{"tmst":56541636,"chan":2,"rfch":0,"freq":915.500000,"stat":...
I'trying STN32WLcube firmware 1.1.0. The LoRaWAN End Node works as aspected and now I need to add my sensors, but when I debug it I have the error "Target is not responding, retrying..."DEBUGGER_ENABLED value is set to 1 ( I think is the same as DEBU...
TLDR; The current tools for BLE in STM32CubeIDE and STM32CubeMX do not work properly for custom BLE profiles in the STM32WB55. When will the tools support it, and when will the documentation be updated with the current system?Firstly, I would prefer ...