STM32 MCUs Wireless

Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NUCLEO-WBA25CE1 "Bootloader limitation"

Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.

ctrois by ST Employee
  • 218 Views
  • 1 replies
  • 1 kudos

Matter software expansion for STM32Cube

Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link  MATTER - Matter software expansion for STM32Cube - STMicroelectronics  It is a reference implementation for the demonstration of Matter on ST...

Ouadi by ST Employee
  • 4064 Views
  • 0 replies
  • 3 kudos

Modification of OTA Control in The Firmware

Hi,I am currently using STM32 custom board with STM32CubeWB. I am a newbee in writing the firmware. There were two versions of binary files I got from previous programmer, one is with OTA function and one is without OTA function. They were uploaded i...

CLIN.4 by Associate
  • 839 Views
  • 0 replies
  • 0 kudos

STM32WB cannot connect to the phone using code from cubemx

I am using STM32WB50 to build a sensor which can be connected by the Android app via BLE. The code is generated by cubemx, and advertise works fine. But it will not work when the phone request a connection with the MCU.I captured the BLE packages wit...

0693W00000APJbLQAX.jpg 0693W00000APJbpQAH.jpg
LZi.1 by Associate
  • 1615 Views
  • 2 replies
  • 0 kudos

SX126x and STM32WL

In ST's documentation, great pains seem to be taken to avoid specifically identifying the Semtech SX126x radio implementation. ST consistently refers to it as a "sub-GHz radio." Why is this?

SWagn.1 by Associate II
  • 957 Views
  • 0 replies
  • 0 kudos

Problems with ADC in LORA Process

Hello,I have problem with ADC using in LORA Porcess on NUCLEO WL55JC1.I modified project PING PONG(from LORA) to MASTER and SLAVE, where SLAVE send to MASTER in periodicly time a voltage form ADC, when I use ADC in main, everything its ok, but when I...

0693W00000DpvPCQAZ.png 0693W00000DplgXQAR.png 0693W00000DplgSQAR.png
MMoro.5 by Associate
  • 931 Views
  • 0 replies
  • 0 kudos

Resolved! STM32WB55 for ZigBee protocol

I would like to send an image of size 320x240 pixels using ZigBee mesh to the intended node from coordinator. What is the maximum range of ZigBee in mesh configuration achieved with STM32WB55 with external SMD antennaWhat is the power consumption in ...

YSN by Senior
  • 2592 Views
  • 7 replies
  • 1 kudos