User Activity

What does the TSC_IOASCR register do?Checked the reference manuals for STM32 WB35xx/WB55xx (RM0434) and F0xx (RM0091) and only get the following information: What's the behaviour of this setting for pins in the various modes (unused, sampling, channe...
I'm trying to use the STM32WB firmware event callbacks defined in ble_events.h and ble_events.c but they don't appear to be working.According to the documentation in PM0271 revision 2 section 4.4 I should be able to use the event callbacks framework ...
Is there a firmware package I can use with the P-NUCLEO-WB55 USB Dongle so that I can use that dongle as a USB BLE Radio? I want to be able to develop a BLE device (Nucleo board) as a bluetooth device but my Windows PC doesn't have a Bluetooth radio ...
Kudos from