Stm32WB55 loses connection due to power issues.
Hi all,
I have the STM32WB55 board connected to a battery. However it loses connection (firmware does continue without issues) quite often. After some research I have found out that when i attach the charger or the st link the disconnection issue is gone. Leading me to believe that the battery isn't capable of supplying enough for the system + ble when transmitting.
So I've added a 36uF polarized capacitor on the 3v3 of the arduino morpho connector to provide for the peaks. This does solve the problem as well.
Now the question:
How big a capacitor do I need to be able to transmit data without losing connection? In the UM2435 user manual stm32wb are some power related schematics. The 5v has a 10uf +100nf and the 3v3 has 1uf and few 100nf....
My hardware knowledge is not good enough to determine the size I need, please help.
Kind regards,
Taxara