STM32 MCUs Wireless

Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NUCLEO-WBA25CE1 "Bootloader limitation"

Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.

ctrois by ST Employee
  • 219 Views
  • 1 replies
  • 1 kudos

Matter software expansion for STM32Cube

Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link  MATTER - Matter software expansion for STM32Cube - STMicroelectronics  It is a reference implementation for the demonstration of Matter on ST...

Ouadi by ST Employee
  • 4065 Views
  • 0 replies
  • 3 kudos

I-CUBE-LRWAN flash optimization

Hi,I need more 4kB of flash memory. Can I achieve this easily and safely by removing some not used functionality in the I-CUBE-LRWAN project?I suppose Lorawan Class B and C featues will not be needed. Can I just exclude this files from the project an...

Marcuka by Associate III
  • 907 Views
  • 0 replies
  • 0 kudos

Resolved! STM32WB Fails on SHCI_C2_BLE_Init

Hello! I'm working with a custom STM32WB10CCU board and can't seem to get BLE working.Here are the details:I have no LSE on the board.. just HSE. I'm configuring RFWKP to HSE/1024 and RTC to HSE/32 (I know that LSE is strongly recommended -.. but fro...

WSH by Associate III
  • 6013 Views
  • 9 replies
  • 1 kudos

Recommended TCXO for STM32WL Design

We design a new product where we use STM32WL microcontroller and in the datasheet ST is recommended to use NT2016SF-32M-END5875A, it was not in stock everywhere. We planned to use the ECS-TXO-20CSMV-320-EY-TR TCXO in our design. Please share your rec...

HVeer.1 by Associate II
  • 1643 Views
  • 1 replies
  • 0 kudos

STM32WLE5CC MCU brick when trying to set Brownout Reset level

GreetingsI have been trying to set the BOR option byte via software in a STM32WLE5CC (as part of a RAK3172 evaluation board), but even following various guides i have not been successful in this endeavor, often resulting in the MCU being bricked and ...

IFant.1 by Associate II
  • 14998 Views
  • 14 replies
  • 0 kudos

SUBGHZ_PHY on STM32WLE5CC

I have a problem with SUBGHZ_PHY on STM32WLE5CC.I have 4 devices as follow:Device1: STM32L0XX device using B-L072Z-LRWAN1(SX1261)Device2: same as Device1Device3: STM32WLE5CCDevice4: same as Device3Device1 and Device2 can communicate with each other. ...

CChow.3 by Associate
  • 961 Views
  • 0 replies
  • 0 kudos

Is there any examples using the Lora E5 ?

Hi I have the Lora E5 development kit from seed, and able to send data to the server using the built in AT commands. I cant seem to find any guides, and basic examples on how to use the built in STM32 and Lora. Can anyone point me to the right pages...

Resolved! [STM32WB] [Zigbee] Node name

Hello,I have ran and modified few examples of applications for Zigbee on Nucleo STM32WB.I have registered my STM32WB as a node of my existing Zigbee network and it works fine.My coordinator indicates me that the Zigbee model of the node is "STM32WB"....

0693W000007YzWJQA0.png
LeoGrany by Associate II
  • 3907 Views
  • 6 replies
  • 2 kudos

Resolved! What is the soldering profile for the STM32WB35CCU6A MCU?

The operating temperature range for the above MCU is -40 to 85 deg C (105 deg C junction). Does it mean that the maximum temperature for soldering is 105 deg C, or does it just mean that the MCU will shut down at 105 deg C? I would appreciate it if y...

VVakh.1 by Associate III
  • 3459 Views
  • 2 replies
  • 0 kudos