STM32 MCUs Wireless

Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NUCLEO-WBA25CE1 "Bootloader limitation"

Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.

ctrois by ST Employee
  • 219 Views
  • 1 replies
  • 1 kudos

Matter software expansion for STM32Cube

Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link  MATTER - Matter software expansion for STM32Cube - STMicroelectronics  It is a reference implementation for the demonstration of Matter on ST...

Ouadi by ST Employee
  • 4065 Views
  • 0 replies
  • 3 kudos

Resolved! Found a bug in the Hardware timerserver source file for STM32WPAN Middleware. If RestartWakeupCounter function is past a zero value in its "Value" parameter, then the function will complete without re-enabling the RTC_WAKEUPTIMER.

The case described occurs when multiple timers are used and one repetitive timer is tiggered right after another repetitive timer. The first code snippet below shows the current implementation and the second shows the fixed code.static void RestartWa...

Targo by Associate II
  • 2826 Views
  • 4 replies
  • 0 kudos

Bugs in Mailbox communication code of STM32WB

Hi, I have found a few bugs in the Mailbox communication code of the STM32WB (which is responsible for letting CPU1 and CPU2 communicate). But other Dual-Core MCUs potentially could have the same bugs.The bugs are not security-critical, but they caus...

0693W00000JOwmEQAT.jpg

Resolved! STM32WB aci_l2cap_coc example

Hello,We're looking for example for BLE connection oriented channel.The SDK does provide the interface aci_l2cap_coc_* , however we were not able to find a single example for its usage not in the SDK nor Googling.Can anyone point me in the right dire...

APort by Associate III
  • 1478 Views
  • 2 replies
  • 0 kudos

Resolved! WB55 Nucleo Board + I-NUCLEO-CN0216 Adapter on SPI 1

Hi Everybody!I'm trying to prototype a force measure application with SD-card on a P-NUCLEO-WB55 Board and I-NUCLEO-CN0216. I'm using the latest CubeIDE.The SD Card work perfectly both on SPI 1 and SPI 2(In my project i'm using SPI 2 for the differen...

Hunhazy by Associate
  • 1791 Views
  • 3 replies
  • 0 kudos

Resolved! Main stack pointer stm32wle5xx

Hii try to figure out, if my main stack pointer is correct. When debug my program, after execute startup.s file the value of msp is 0x20008000, but like this i used only half sram, right? This micro have 64KB of sram. I believe that the value of msp ...

en by Associate II
  • 4472 Views
  • 6 replies
  • 0 kudos

Sigfox - trouble at t'mill

In the news today:"Sigfox, the French IoT startup that had raised more than $300M, files for bankruptcy protection as it seeks a buyer"https://techcrunch.com/2022/01/27/sigfox-the-french-iot-startup-that-had-raised-more-than-300m-files-for-bankruptcy...