Skip to main content
Todd Rylaarsdam
Associate
July 15, 2021
Question

How do you configure the transmission frequencies in STM32Cube Lora AT Slave example project?

  • July 15, 2021
  • 2 replies
  • 1432 views

I'm working on getting the STM32WL on a Nucleo-WL55JC1 devboard to reliably communicate with my gateway (a RAK7243), however I'm running into a few issues.

When transmitting from the devboard on the US915 band, I can see the transmission appear on an oscilloscope, so I know the board is transmitting. However, unless the 32WL transmits at nearly the exact frequency I configured the gateway to receive on the transmission never gets forwarded to my backend (chirpstack).

I contacted RAK and they said this gateway was capable of receiving on all 8 channels for the US simultaneously, and that I needed to configure my channel plans on the end node. When I searched the Lora AT example project for channel plan configuration, I only found options for the Australian band, and nothing in the US.

So my question really is: what am I missing here? I see the end node transmitting on varied frequencies, but my gateway only picks up one frequency even though it should pick up the entire US TX spectrum.

Also, is there a way for me to force the STM32WL to transmit on that one frequency? If I were to do that, how many devices would I be able to have on a network transmitting on just that one frequency?

This topic has been closed for replies.

2 replies

Todd Rylaarsdam
Associate
July 16, 2021

bump

LCHAM.1
Visitor II
July 20, 2021

Hello,

In Lora AT_Slave project, you should first verify that in LoRaWAN_AT_Slave\LoRaWAN\Target\lorawan_conf.h, #define REGION_US915 is enabled.

Then, if you want to transmit on one single frequency, this point is already answered in ticket: https://community.st.com/s/question/0D53W00000wxvvTSAQ/i-couldnt-activate-my-stm32wl55jc1-with-single-channel-gateway-draginolg02-via-abp-mode-lora-network-problem-is-how-to-configure-the-device-to-transmit-packets-in-just-1-channel

You should adapt in your case, modifying RegionUS915.h