STM32 MCUs Wireless

Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NUCLEO-WBA25CE1 "Bootloader limitation"

Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.

ctrois by ST Employee
  • 218 Views
  • 1 replies
  • 1 kudos

Matter software expansion for STM32Cube

Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link  MATTER - Matter software expansion for STM32Cube - STMicroelectronics  It is a reference implementation for the demonstration of Matter on ST...

Ouadi by ST Employee
  • 4064 Views
  • 0 replies
  • 3 kudos

Resolved! Custom Lorawan_End_Node application

Hello,So I already downloaded the Lorawan_End_Node example into my Nucleo board and I could see how it works with the TeraTerm terminal.However, now I'm trying to generate a new code from the .ioc file with the CubeMX (I only added the debugger optio...

0693W00000NrviSQAR.png 0693W00000NrvicQAB.png
AZube.2 by Associate III
  • 1437 Views
  • 1 replies
  • 0 kudos

BLE problem with STM32WB55CG

Hi, Everyone. I have encountered a problem in using BLE with STM32WB55CG. I made custom STM32WB55CG board and the schematic is below.When I was testing the functions of the MCU, there was an abnormality in the BLE function. All other peripherals work...

0693W00000NruqGQAR.jpg
Kyuns.2 by Associate II
  • 923 Views
  • 1 replies
  • 0 kudos

P_NUCLEO_WB55 USB_DONGLE(MB1293C) Projects: BLEHeartRate I do as the ' readme.txt'. I can't found the HRSTM in the device list.

step1: I upgrade the firmware 1.2.0 and flash the wireless stack  "stm32wb5x_BLE_Stack_full_fw.bin " .step2: Rebuild all files and flash the board with the executable file.step3: Power On MB1293C and download the ST_BLE_Sensor. But i can't find the H...

Lep by Senior
  • 1430 Views
  • 1 replies
  • 0 kudos

Hello ST Community, I am facing an issue with Bluetooth communication in STM32WB. Sometimes BT disconnected with a custom application.

-The MCU is running well but The Bluetooth is disconnected from the Application. and then restarts the application. BT connects with the App.-is this a hardware side issue or an application issue?Please share your best knowledge.#STM32WB​ #BT #BLE​ #...

Sagar1 by Associate II
  • 1244 Views
  • 2 replies
  • 0 kudos