2022-06-11 3:52 AM
-The MCU is running well but The Bluetooth is disconnected from the Application. and then restarts the application. BT connects with the App.
-is this a hardware side issue or an application issue?
Please share your best knowledge.
#STM32WB #BT #BLE #BLE_Disconnetcted
Thanks
Sagar
2022-06-13 9:37 PM
You are presenting a very nebulous problem in kind of a lazy way - you should start with something that is working out-of-the-box, like an ST sample application running on ST demo hardware, like the STM32WB Nucleo board, and connecting to an ST sample application on the Android - like the HeartRate monitor example, end-to-end. Then you add your customizations little by little while keeping everything working.
2022-06-14 5:21 AM
Hello,
Can you give more information about your setup ? Which BLE stack and which version are you using ? What are you doing in your custom application ?
Best Regards