STM32 MCUs Wireless

Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NUCLEO-WBA25CE1 "Bootloader limitation"

Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.

ctrois by ST Employee
  • 218 Views
  • 1 replies
  • 1 kudos

Matter software expansion for STM32Cube

Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link  MATTER - Matter software expansion for STM32Cube - STMicroelectronics  It is a reference implementation for the demonstration of Matter on ST...

Ouadi by ST Employee
  • 4064 Views
  • 0 replies
  • 3 kudos

How to migrate from a TCP WiFi data server to BLE data server

Hello everyone,I want to migrate my existing TCP-WLAN based MCU application which acts as a data server with a proprietary protocol. The application comes very close to standard Posix TCP handling. Each connection is handled by a separate thread that...

Edmund by Associate II
  • 691 Views
  • 0 replies
  • 0 kudos

STM32WB55RG: Instability of LSE clock on Nucleo board

Hi,I am using the Nucleo WB55 board that has a STM32WB55RGV6 MCU to develop an application. I see instabilities in bluetooth by default when I am using the LSE clock as RfWkUpClock of the BLE that are leading to the BLE core crashing.Those instabilit...

apous.1 by Associate II
  • 2458 Views
  • 3 replies
  • 0 kudos

how can i use stm32wl55jc to transmit CW beacon?

I have nucleo-wl55jc board i want to transmit CW beacon.i am able to transmit continuous wave but not able to sleep the radio and continue next transmit.What would be the possible way to start and stop radio quickly?

scora.1 by Associate
  • 1228 Views
  • 1 replies
  • 0 kudos

Resolved! no Radio Rx timeout after the Radio.Rx function called?

Hi, I create my new project follow the SubGHz Phy Ping Pong example project.In the example project, the RTC configure in "Free running Binary mode". In my project, I configure the RTC in "Free running BCD calender mode" therefore no Radio Rx Timeout ...

no radio Rx timeout after Radio.Rx() called

Hi,I use STM32WLE5CBU6. I created SubGHz Phy project. Device entered stop 2 mode, exit stop 2 mode when the alarm B interrupt issue then the Radio.Rx(3000) is called to receive data.my RTC Alarm interrupt function below,void HAL_RTCEx_AlarmBEventCall...

Hi, I'm trying to understand how storing and restoring the LoRa context for stm32wl works. To my understanding it would be ossible to skip the join process if the device is already joined once even if it is power cycled?

I've made sure "force rejoins at reboot" is not not ticked in the configuration file, and then I set the task "LoRaStoreContextEvent" in the beginning of the user code section like thisstatic void OnNvmDataChange(LmHandlerNvmContextStates_t state) {...

ABläs.1 by Associate II
  • 2174 Views
  • 2 replies
  • 0 kudos