Skip to main content
NK_it
Associate III
November 15, 2021
Question

P-NUCLEO-WB55 Nucleo RF kit: Can not start project using STM32CubeMX

  • November 15, 2021
  • 1 reply
  • 755 views

Not able to start project in STM32CubeMX after board selection of P-NUCLEO-WB55 RF kit.

Do we require any license for this?

Please provide information for the same.

Thanks!

This topic has been closed for replies.

1 reply

Yaroslav Vushnevsky
Associate II
November 30, 2021

No licence needed. It is just bugged soft. Use "Example selector" option to start your project from example.

Yesterday was update, but it still pain in the ***. You cant configure debug UART in clean project, because option just inactive without reason. They know about bug about half of the year and do nothing. More over - now version of libraries are 1.13.0, but when you try to start project from example - CubeIde download 1.12.1 and start project from it. WHAT THE ****!