STM32 MCUs Wireless

Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NUCLEO-WBA25CE1 "Bootloader limitation"

Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.

ctrois by ST Employee
  • 218 Views
  • 1 replies
  • 1 kudos

Matter software expansion for STM32Cube

Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link  MATTER - Matter software expansion for STM32Cube - STMicroelectronics  It is a reference implementation for the demonstration of Matter on ST...

Ouadi by ST Employee
  • 4064 Views
  • 0 replies
  • 3 kudos

Use of STM32CubeIDE with LoRaWAN_End_Node: create a project.

I'm working with STM32CubeWL, version 1.1.0. Starting a new project from .ioc file seems that the firmware will be upgraded to the version 1.2.0. Is this correct? Can I find, somewhere in the source code, the firmware version?Can I avoid this behavio...

0693W00000Su0mEQAR.png
FRest.1 by Associate III
  • 3418 Views
  • 5 replies
  • 0 kudos

Resolved! How to install STM32CubeWB from STM32CubeMX

HiI am trying to install STM32CubeWB from STM32CubeMX by following YouTube "STM32WB Getting Started Series: Part 3, Tools Install". After clicking "INSTALL/REMOVER" button, I got message "The Updater is already in use and checking the server. Please ...

NWang.2 by Associate II
  • 1563 Views
  • 1 replies
  • 0 kudos

STM32WB5M BLE MESH LIBRARY can not find unprovisioned device

I am trying to build an embedded provisioner for the stm32wb5m, but i am not able to find an unprovisioned device.I am using the example "BLE_MeshLightingProvisioner" for the WB55 nucleo Board as reference.The Initialization of the STM32WB and the co...

CBuch.1 by Associate III
  • 1390 Views
  • 1 replies
  • 0 kudos

Resolved! WHY PER CALCULATION DOES NOT WORK AS EXEPTED?

Hi, following your DS, LoRa PER = 1%. While RF examination, for BW= 125KHz and SF=7, the sensitivity of the micro controller is around -125dBm for PER = 1%. When we change the value of SF to 12, the sensitivity should change to -138dBm but in reali...

TLit.1 by Associate
  • 1955 Views
  • 2 replies
  • 0 kudos

I-NUCLEO-LRWAN1 - AT command issue

Hello,I am using I-NUCLEO-LRWAN1 development kit for LoRa setup. I have interfaced that setup with USB module and I am trying to communicate it using X-CTU. When I start the module the module sends #, but it's not responding to AT<CR>. I have attache...

HDesa.1 by Senior
  • 1011 Views
  • 0 replies
  • 0 kudos

Resolved! How to get Vbat and Internal temperature ?

Hello, I am using a p-Nucleo-wb55. I would need to get data from vbat channel and the internal temperature channel. I used the example for internal temperature and it works but I am not able to add the reading of vbat value. Am I supposed to use one ...

0693W00000QNtNoQAL.png
LVolp.2 by Associate II
  • 3240 Views
  • 5 replies
  • 0 kudos