STM32 MCUs Wireless

Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NUCLEO-WBA25CE1 "Bootloader limitation"

Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.

ctrois by ST Employee
  • 218 Views
  • 1 replies
  • 1 kudos

Matter software expansion for STM32Cube

Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link  MATTER - Matter software expansion for STM32Cube - STMicroelectronics  It is a reference implementation for the demonstration of Matter on ST...

Ouadi by ST Employee
  • 4064 Views
  • 0 replies
  • 3 kudos

STM32 WB BLE event handling

I put a debug message at the beginning of my event handler but the only event value I see is 0xFF. hci_event_pckt *event_pckt;evt_blecore_aci *blecore_evt;event_pckt = (hci_event_pckt *)(((hci_uart_pckt*)Event)->data);BLE_DBG_EEG_MSG("EEG Event %d re...

EHD by Associate II
  • 1560 Views
  • 1 replies
  • 0 kudos

Resolved! [STM32WB55] How to use CHAR_PROP_WRITE modified in sample code

Hi Sir,​I use sample code in STM32Cube_FW_WB_V1.13.0\Projects\P-NUCLEO-WB55.Nucleo\Applications\BLE\BLE_p2pServer and BLE_p2pClient. The BLE characteristic's property CHAR_PROP_WRITE_WITHOUT_RESP is used in the sample, I try to modified it as CHAR_PR...

LChan.5 by Associate II
  • 1585 Views
  • 1 replies
  • 0 kudos

About lora repeater

Can i use any stm32 mcu chip which used as lora repeater?Because i need in my project.Also give source code if available.

PPraj.1 by Associate II
  • 1332 Views
  • 1 replies
  • 0 kudos

Acess ADC data from a STM32WBxx front end radio

Hello! I was wondering if it's possible to access some more raw RF data from your STM32WBxx product. I would like to have access to some I/Q data before those be converted into digital BLE packets. I thought a good first step could be to have access ...

0693W00000QO9gSQAT.png
ALope.1 by Associate II
  • 1922 Views
  • 3 replies
  • 0 kudos

How to change the Data rate for sending more than 11 bytes using I-CUBE-LRWAN? #LoRaWAN #I-CUBE-LRWAN #B-L072Z-LRWAN1

We are using B-L072Z-LRWAN1 for developing our application. We are struggling to send more than 11 bytes of application payload. As long as the total payload is 11 bytes, the node joins the network with no issues. When we try to change the DR > 0 so ...

sid1 by Associate II
  • 1927 Views
  • 3 replies
  • 1 kudos

STM32WL End Node RTC BCD Calendar Mode

Hello,I'd like to know if it's possible to use RTC with a BCD Calendar mode with the end node example. Indeed, I've tried to, but it seems that the timer server doesn't work when i'm not using the binary mode.Thanks !

MLour.1 by Associate
  • 1006 Views
  • 1 replies
  • 0 kudos

How to set up BLE AT Client on B-U585I-IOT02A?

Hello!I'm attempting to set up the BLE AT Client example in the STM32U5 firmware package on a B-U585I-IOT02A board. I've managed to flash it, but when I run it on the debugger (through the ST-Link v3 USB port), the "AT" and "AT+BLE_SVC=1" commands se...

juyec by Associate II
  • 2134 Views
  • 2 replies
  • 0 kudos

Resolved! Code generation glitch for RTC with STM32WL

I think I have had the same issue as: https://community.st.com/s/question/0D53W00001Z9hswSAB/code-generation-problem-for-rtc-with-stm32wlHowever that thread never got answered so I post again, this time with additional information.Im using STM32CubeI...

0693W00000QNdk8QAD.png 0693W00000QNdkIQAT.png 0693W00000QNdkSQAT.png 0693W00000QNdkXQAT.png
AAlat.1 by Associate II
  • 1993 Views
  • 2 replies
  • 1 kudos