NUCLEO-WBA25CE1 "Bootloader limitation"
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link MATTER - Matter software expansion for STM32Cube - STMicroelectronics It is a reference implementation for the demonstration of Matter on ST...
Please go and visit our wiki pages where you can find a lot of information on our wireless product families (WB, WBA, WL) and the supported protocols: BLE, Zigbee, Thread, Matter, Lora, ... To begin your technical journey, please start from this top ...
Details in the SECoreBin/readme.txt file for the STM32WB code says that the MCU needs to be booted with PH3-BOOT0 pulled high in order to program the Authentication Key. I can't find any other documentation that indicates that this is true. Does the ...
Hi,is there any option to set different tx power level (aci_hal_set_tx_power_level) when device is connected and is still advertising in background? My goal is to set minimum tx power level for advertising and maximum for connection, when both states...
I expirence very strange behavior on STM32WB. After 6 connect/disconnect sequences, CPU2 stops working. I'm not receiving any IPPC interrupts. Last event I get, before CPU2 stuck, is ACI_ATT_EXCHANGE_MTU_RESP_VSEVT_CODE. I tried to call hci_reset fun...
On the website I can only download the latest version (2.1.0 in this case)We are working on a project that uses version 1.3.0 + our custom changes and we want to get version 1.3.0 to differentiate the original from our changes
I've been doing some current draw analysis of our product and I am trying to get the best idle current that I can get. We have a mode where there is no BLE connection and no advertising. Essentially no BLE communication at all. In this mode I woul...
Hello,I used a GFSK configuration with 433MHz and it is work very well,I try now to migrate to Lora modulation. i used a basic config, but the receiver on the other side receive less then 1% of sent frames ! (even transmitter and receiver are very cl...
I am trying use the stm32wb15cc to run an application on CPU1, but with no application in CPU. I don't need the RF side at all and want to hold CPU2 in reset and allow CPU1 to access all the Flash and Ram.However this does not seem possible as Option...
I attended the Tuesday Sept 7th session of the lorawan-with-stm32wl-soc-workshop-ame-2021 I was unable to complete the workshop during the allotted time. I would like to complete the training. Are the videos available?
Hello,we are developing an application with LoRaWAN and FreeRTOS, based on STM32CubeWL, for a custom board.While we got this to send data properly with the LoRaWAN "End Node skeleton", we are facing issues with the "User defined skeleton".With "User ...
Hi all,I have recently started working on B-L072Z-LRWAN1 for understanding the LoRaWAN protocol.I am using icube lrwan software for example code.I was able to build the code successfully.But when tried to flash the code using openocd,i am continuousl...