2022-01-25 3:32 AM
Hi all,
I'm trying to implement SPI TX communication with DMA.
The following "prepareDMASPI()" function should configure and start DMA transferts from a buffer to the SPI device.
But it doesn't work (No spi clock or MOSI data), although the SPI is properly configured
(and working when used without DMA)
Could you please tell me if you see something missing ?
(It's Go code, but should be easy to understand)
Thanks.
func prepareDMASPI() {
// Disable device, memory to memory mode, peripheral increment
stm32.DMA1.CCR1.ClearBits(stm32.DMA_CCR1_MEM2MEM | stm32.DMA_CCR1_PINC | stm32.DMA_CCR1_EN)
// Set Memory increment, circular mode, memory to peripheral
stm32.DMA1.CCR1.SetBits(stm32.DMA_CCR1_MINC | stm32.DMA_CCR1_CIRC | stm32.DMA_CCR1_DIR)
stm32.DMA1.CCR1.ReplaceBits(stm32.DMA_CCR1_MSIZE_Bits8, stm32.DMA_CCR1_MSIZE_Msk, 0) // 8bit mem mode
stm32.DMA1.CCR1.ReplaceBits(stm32.DMA_CCR1_PSIZE_Bits8, stm32.DMA_CCR1_PSIZE_Msk, 0) // 8bit periph mode
stm32.DMA1.CCR1.ReplaceBits(stm32.DMA_CCR1_PL_High, stm32.DMA_CCR1_PL_Msk, 0) // High priority
stm32.DMAMUX.C0CR.ReplaceBits(stm32.DMAMUX_C0CR_DMAREQ_ID_SPI1_TX_DMA, stm32.DMAMUX_C0CR_DMAREQ_ID_Msk, 0) // Route DMA to SPI1 TX
stm32.DMA1.CMAR1.Set(uint32(uintptr(unsafe.Pointer(&ws2812_buffer[0])))) // Memory address
stm32.DMA1.CPAR1.Set(uint32(uintptr(unsafe.Pointer(&machine.SPI0.Bus.DR)))) // Periph. data register addr
stm32.DMA1.CNDTR1.Set(WS2812_BUFFER_SIZE) // Transfert size
stm32.SPI1.CR1.ClearBits(stm32.SPI_CR1_SPE) // Disable SPI
stm32.SPI1.CR2.SetBits(stm32.SPI_CR2_TXDMAEN) // Tx Buffer DMA
stm32.SPI1.CR1.SetBits(stm32.SPI_CR1_SPE) // Enable SPI
stm32.DMA1.CCR1.SetBits(stm32.DMA_CCR1_EN) // Enable DMA1 Channel 1
}
Solved! Go to Solution.
2022-01-25 5:13 AM
Hi,
So stupid ....
You were right : I forgot to enable clock
The above code is now working, as soon as you add the clock enable at the beginning of the function !
// Enable DMA/DMAMUX clocks
stm32.RCC.AHB1ENR.SetBits(stm32.RCC_AHB1ENR_DMAMUX1EN | stm32.RCC_AHB1ENR_DMA1EN)Thanks for your help.
2022-01-25 3:46 AM
> It's Go code, but should be easy to understand
Regardless, it may be reason for problems. Also, we don't see rest of the program - maybe it's gotcha #1 - no peripheral (e.g. DMA) clock.
Read out and check/post SPI, DMA and DMAMUX registers content.
JW
2022-01-25 5:13 AM
Hi,
So stupid ....
You were right : I forgot to enable clock
The above code is now working, as soon as you add the clock enable at the beginning of the function !
// Enable DMA/DMAMUX clocks
stm32.RCC.AHB1ENR.SetBits(stm32.RCC_AHB1ENR_DMAMUX1EN | stm32.RCC_AHB1ENR_DMA1EN)Thanks for your help.