User Activity

Hi all, I'm trying to implement SPI TX communication with DMA. The following "prepareDMASPI()" function should configure and start DMA transferts from a buffer to the SPI device. But it doesn't work (No spi clock or MOSI data), although the SPI is pr...
Hi, I have a  Nucleo-wl55jc2 (US Low Band 433 Mhz) Would it be possible to remove the RF filters so I can run it on high frequences (EU 868 Mhz) ? Thanks Olivier
I bought NUCLEO-WL5JC2 Low Band (As NUCLEO-WL5JC1 were not in stock)Is it possible to turn them into High Band by changing some passive components ? So I can use them in 868Mhz instead of 433Mhz Thanks
Hi all. I found out there are specific DEBUG_SUBGHZSPI_* alternate functions (DS13105 STM32WLE5xx). But there is not much information about these functions. Can these AF be used to 'mirror' SUBGHZSPI pins for debugging / captures ? Thanks Olivier...
Hi all. I'd like to write a simple bare-metal application for STM32WLE5JC. Could you provide snippet code for STM32WL (core + radio) initialization and simple RX/TX Lora Packet ? Thanks Olivier
Kudos from