STM32 MCUs Wireless

Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NUCLEO-WBA25CE1 "Bootloader limitation"

Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.

ctrois by ST Employee
  • 218 Views
  • 1 replies
  • 1 kudos

Matter software expansion for STM32Cube

Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link  MATTER - Matter software expansion for STM32Cube - STMicroelectronics  It is a reference implementation for the demonstration of Matter on ST...

Ouadi by ST Employee
  • 4064 Views
  • 0 replies
  • 3 kudos

Resolved! Sigfox and LoRa AT commands for STM32WL5MOC

The STM32WL5MOC component is both LoRaWAN and Sigfox verified. I need to be able to use both types of connections. AT commands for LoRaWAN are readily available. Is there a guide of AT commands for Sigfox and an AT command to switch between modes? Th...

Resolved! STM32WL5MOC power consumption

Hello,I'm looking to measure the power consumption of the STM32WL5MOC component on a B-WL5M-SUBG1 development board.I'm looking for the power consumption announced by the Sleep Mode datacheet (140nA - 810nA).I connected directly to JP2 to use only ST...

alexemdesgagne_0-1712602977112.png

Boot problem in STM32WLE5

Hello ST, We are using the STM32WLE5 controller in our product.The system always works on 1.8V. Based on demand, we switch to 3.3V and fallback to 1.8V.Our product is IoT-based, charged through solar to a supercapacitor.The main problem is that the c...

kalpeshDryad_0-1763066406831.png IMG_6364.jpg

Resolved! STM32WBA54 SAI Slave mode DMA cannot stop and reinitiate

STM32WBA54 SAI work in slave mode with DMA: SAI1_Block_A Slave out, SAI1_Block_B Slave in. test code as:  MX_SAI1_Init();//in  __HAL_LINKDMA(&hsai_BlockB1, hdmarx, handle_GPDMA1_Channel2);  MX_RxQueue_Config();  HAL_DMAEx_List_SetCircularMode(&RxQueu...

HuangFan by Associate II
  • 584 Views
  • 3 replies
  • 0 kudos

Resolved! STM32WB5MMGH6TR full datasheet missing...?

Hi, we are designing a product around the STM32WB5MMGH6TR but cannot find a full datasheet.On the product page we can find what is described as a datasheet (main purple download button at the top) but is only a 37 pages "technical brochure" that does...

Ricko by Senior III
  • 577 Views
  • 4 replies
  • 4 kudos

STM32WL and LoRaWAN Endnode example - resets occuring

I am new to the NUCLEO WL55JC1 and wanted to experiment with LoRaWAN.I've followed the YT series on the topic, especially the 3rd part (https://www.youtube.com/watch?v=8KNfrWoa1fw&t=26s). My End node is properly joined and connected to the things net...

MDaub.1 by Associate III
  • 370 Views
  • 0 replies
  • 0 kudos

Resolved! STM32WB5 transparent mode issue

Hello everyone, I am strugling with a STM32WB5MMGH that I am using with transparent mode. I am using the STM32WB5MMGH on a custom board with a STM32L4R9VIT6. The goal of the project is to use the STM32WB5 as a bridge to send data from a smartphone ap...