STM32 MCUs Wireless

Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NUCLEO-WBA25CE1 "Bootloader limitation"

Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.

ctrois by ST Employee
  • 218 Views
  • 1 replies
  • 1 kudos

Matter software expansion for STM32Cube

Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link  MATTER - Matter software expansion for STM32Cube - STMicroelectronics  It is a reference implementation for the demonstration of Matter on ST...

Ouadi by ST Employee
  • 4064 Views
  • 0 replies
  • 3 kudos

Custom board Stm32WBA65RIV6 no DFU connection

Hello everyone, I'm writing in search of some help, as I'm not sure what else to check. I have just built a custom board controlled by an STM32WBA65RIV6, and I'm trying to connect it via DFU mode. Everything seems to be set up correctly, but the devi...

STM32WL33 µC on IAR Embedded IDE 9.30

Hello,I would like to build a project using a STM32WL33 µC on IAR Embedded Workbench IDE v9.30.1. Unfortunately, this version of IAR does not support this µC and I would like to import it but i cannot find any package suitable for IAR. Do you have an...

GScha.1 by Associate II
  • 285 Views
  • 1 replies
  • 0 kudos

Resolved! STM32WLE5 Exit stop mode 2 on EXTI or RTC timer

I cannot get STM32WLE5 (on a RAK3172 module) to exit from stop mode on either RTC timer or rising EXTI pin. I'm using STM Cube HAL functions and the stm32_lpm_if.c library. I have tried pin PB3 as either  EXTI3 or as PWR_WKUP3. If I use EXTI3, I set ...

SLevi.1 by Senior
  • 2519 Views
  • 6 replies
  • 0 kudos

Resolved! STM32WBA65 USB Phy Clock power usage

Hello,I am working with an STM32WBA65RI that is on our custom board, and working to reduce our power usage. Along this journey I found the issue with the HAL_PCD_MspInit() / DeInit() where the logic for the RCC PWR was inverted, which was another pos...

JFisherLegato_1-1761241661788.png JFisherLegato_0-1761240882377.png

stm32wba65, BLE and RTC timer not firing

I have a set of BLE characteristics set up, and working ok. The project uses FreeRTOS. I want to be able to have the stm32wba65 sleep in low power, then wake up at a specific time of day. After wakeup,I have a 5-second RTOS timer to take a series of ...

SLevi.1 by Senior
  • 357 Views
  • 0 replies
  • 0 kudos