2025-03-27 2:13 PM
Hi all,
I've adapted stm32loader python script to working with STM32WL familly, https://github.com/copterust/stm32loader/blob/master/stm32loader.py .
It's working I'm able to flash, read, erase flash. I can flash my firmware. But for now I'd like to reboot my STM after flashing my firmware, but I don't underqtand well if I can do it.
I've find some post, but no usefull information, in the python script I have this parameter :
-g address Start executing from address (0x08000000, usually)
But if I try to use it, nothing happend, I have to reset manually ùy STM for reboot.
2025-04-08 12:01 AM - edited 2025-04-08 12:02 AM
A response on this topic would be very interesting to me as well! Also by using STM32CubeProgrammer I was not able to directly run the firmware when using UART for flashing.
2025-04-29 8:26 AM
Hello @SBaro.11
The link you are mentioning is not for an ST Official repository. So, i could not confirm if it is going to work or not.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.