2025-04-27 5:20 PM
When generating code that uses the CMSIS OS V2, it appears that a template directory gets included in the generated code. causing massive linker errors.
The offending directory is Drivers/CMSIS/Device/ST/DEM32WL3X/Source/Templates. Removing it gets rid of the errors.
While we are at it, the LICENSE.txt file in the same directory is spelled incorrectly, it should be LICENCE.txt, as it is not a verb.
Solved! Go to Solution.
2025-04-28 1:33 AM
Hello @divmstr
I'm not able to reproduce this behavior. Could you please test it using the STM32CubeMX V6.14.1 and the STM32CubeIDE V1.18.1 and give me the file that reproduce this issue if it is reproduced on your side.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2025-04-28 1:33 AM
Hello @divmstr
I'm not able to reproduce this behavior. Could you please test it using the STM32CubeMX V6.14.1 and the STM32CubeIDE V1.18.1 and give me the file that reproduce this issue if it is reproduced on your side.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.