STM32 MCUs Wireless

Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NUCLEO-WBA25CE1 "Bootloader limitation"

Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.

ctrois by ST Employee
  • 218 Views
  • 1 replies
  • 1 kudos

Matter software expansion for STM32Cube

Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link  MATTER - Matter software expansion for STM32Cube - STMicroelectronics  It is a reference implementation for the demonstration of Matter on ST...

Ouadi by ST Employee
  • 4064 Views
  • 0 replies
  • 3 kudos

STM32WB55 FATFS sd real time

The stm32wb55 writes data to the sd card in real time through FATFS, and the function f_write() will take tens of ms. I want to use two buffers, one buffer to store data, and one buffer to write data to and from the sd card (can this avoid the delay ...

Lep by Senior
  • 4415 Views
  • 9 replies
  • 1 kudos

Problem cloning STM32WB55 BLE_p2pServer example

I have a custom board running the STM32WB55. My medium term goal is to use BLE to perform OTA updates for my firmware. I'm trying to leverage the BLE_p2pServer BLE_p2pServer_ota examples from the as a starting point, but I'm getting stuck at one o...

Resolved! Unable to wakeup from stop mode with LPTIM

Hello, I have a STM32WLE5JB, and a want to wakeup the chip from sleep mode to have multiple task. (Read a sensor every x sec) externally from the RTC that is tied to the lora TX delay.So i have the code that include the lora stack without any modific...

HDIA.1 by Associate III
  • 7348 Views
  • 9 replies
  • 0 kudos

STM32WL rfbusys

On STM32WL is the rfbusys only available in polling mode or is there an interrupt linked to it ?

FGERA.1 by Associate
  • 773 Views
  • 0 replies
  • 0 kudos

Flash Operations Initializations.

Hi Team,We are using the STM32WB55 Series for our project. We are using specific flash sectors (8) for our config data. Is there any specific Initializations are required for Flash Operations which is similar to other peripherals like Clock, UART, I2...

STM32WB55 Comparator max speed

I have a board NUCLEO-WB55 and I'm testing some examples.I'd like acquire a sine wave about 14 MHz and convert to square wave with internal comparator. I can't find enough informations on datasheet if it's fast to acquire this signal.Thank you for su...

juvann by Associate III
  • 1074 Views
  • 1 replies
  • 1 kudos