STM32 MCUs Wireless

Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NUCLEO-WBA25CE1 "Bootloader limitation"

Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.

ctrois by ST Employee
  • 218 Views
  • 1 replies
  • 1 kudos

Matter software expansion for STM32Cube

Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link  MATTER - Matter software expansion for STM32Cube - STMicroelectronics  It is a reference implementation for the demonstration of Matter on ST...

Ouadi by ST Employee
  • 4064 Views
  • 0 replies
  • 3 kudos

Need I2C Code base with 1 Fast Mode

Hi Team,We are using the I2C Bus to read the Eeprom Data. We configured with 100Khz speed with DMA to transfer the data.After initialization of I2C and DMA it is working fine and able to Read and write the data with different speeds.If we read the da...

Resolved! How can enable the SYSCFG in STM32WB55RGV6

Hi,I want to enable the SYSCGF in STM32WB55RGV6 , but when ı look the reference manuel; it says that SYSCFG is on the APB2 bus however when look the APB2ENR register there is nothing about SYSCFG . What should ı do to enable SYSCFG?

MOB1 by Associate II
  • 2193 Views
  • 2 replies
  • 1 kudos

Manage RF power

Hello.I have a STM32WLE5LB that has both RF LP and RF HP but leaving the settings as default in DR0 the device consume up to 80mA . That means that only the RF HP is used.How change this ?Also my gateway : Kerlink Fetmocell seems to don't have ADR se...

HDIA.1 by Associate III
  • 1771 Views
  • 2 replies
  • 0 kudos

Serial Wire debug Nucleo-WL55 JC1 SWO

Hi, I trying to debug on nucleo-WL55 with serial wire debug via SWO. I have enable "Serial Wire Viewer (SWV)" in debug config, and add SWV ITM Data console (Config 0).Even add this code : int _write(int file, char *ptr, int len) { /* Implement your...

0693W00000WKERiQAP.png 0693W00000WKESHQA5.png 0693W00000WKERxQAP.png
LEdou.1 by Associate III
  • 7693 Views
  • 17 replies
  • 1 kudos

Simple exemple multiple channel ADC

Hello, I'm Using the STM32WLE5JB with STMCubeWL , and i'm wondering how i need to confirgure the .ioc and writing the code to have a arduino style ADC.Without DMA i want to read only the channel that i want to read and not all in one time.I tried som...

HDIA.1 by Associate III
  • 1503 Views
  • 1 replies
  • 0 kudos