STM32 MCUs Wireless

Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NUCLEO-WBA25CE1 "Bootloader limitation"

Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.

ctrois by ST Employee
  • 218 Views
  • 1 replies
  • 1 kudos

Matter software expansion for STM32Cube

Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link  MATTER - Matter software expansion for STM32Cube - STMicroelectronics  It is a reference implementation for the demonstration of Matter on ST...

Ouadi by ST Employee
  • 4064 Views
  • 0 replies
  • 3 kudos

Utility Sequencer not starting task

Apologies for cross post, I couldn't find a way to delete the other post or how to change which board to post it to.I'm trying to set up the Utility Sequencer to run an acquisition task followed by an signal processing task, see code snippets below.W...

Design for STM32WL55CC + 22dbm, 868MHz

Hello,I am currently designing a custom PCB with the STM32WLE5CC (QFN package) targeting +22 dBm in the 868 MHz frequency band.I have been following the reference design based on the MB1720 board, which is specifically described as being for +22 dBm ...

blnc___0-1763975427911.png
blnc__ by Associate II
  • 458 Views
  • 0 replies
  • 0 kudos

Resolved! LORA-E5-HF(stm32wle5jc)

Respected Sir/ Madam,    AS i'm using LORA-E5(stm32wle5jc) module communicating point to point Radio Frequency and AT Command also. We are config SubGHz for Radio Send and Receive Functions in Loop Mode . No Response received from this.  By using AT ...

SYAMALA by Associate II
  • 3465 Views
  • 6 replies
  • 0 kudos

STM32WLE5JCI6 with LoRa-E5 Development Kit.

Hi techs, I have a problem with the LoRa configuration with the LoRa-E5 Development Kit. How to do the Pin configuration for the LoRa point to point communication. I have tried multiple ways to do but the communication is not happening, and I also tr...

RTC Calendar STM32WBA65

I am trying to modify the BLE_HeartrateFreeRTOS project. I will set the RTC date/time from a timestamp received over BLE from a PC. I need the RTC calendar to be running, as I need to timestamp data readings with a "Unix" timestamp. I also need to pe...

SLevi.1 by Senior
  • 488 Views
  • 1 replies
  • 0 kudos

STM32WL5MOC with external antenna

Hi all,I designed a sensor board with STM32WL5MOC based on B-WL5M-SUBG1. Due to other constraints I cannot place the antenna directly on the PCB. Therefore I would like to place an U.FL connector (like: https://www.digikey.hu/en/products/detail/hiros...

STMWB05N: SMP/Pairing Request does not trigger.

Hello, I am using STM32H735 and installed a Bluetooth module STM32WB05N. For the STM32WB05N, it is configured as a transparent mode running as HOST + CONTROLLER firmware.  I got the firmware from this github: STM32WB05N Firmware. I have modified STM3...

rsatina by Associate
  • 546 Views
  • 0 replies
  • 0 kudos

STM32 WB55RG sudden fail

-------------------------------------------Board: STM32 WB55RGOS: Ubuntu 25.10 questingKernel: x86_64 Linux 6.17.0-6-genericSTMCubeProgrammer Version: v2.21.0-------------------------------------------I recently noticed that my board was not being fl...