User Activity

I would like to be able to turn BLE off (e.g. with a timer) even if it is currently connected. I know I can stop it advertising, but this doesn't seem to kill the connection. Basically, after a timeout, I would like the BEL to shutdown and stop using...
Apologies if this has already been answered elsewhere, I had a search and all I could find was an old discussion about TrueStudio not doing it and it didn't really go anywhere.Simple question, is there a way to setup the option bytes (BOOT0,1, etc.) ...
TLDR; The current tools for BLE in STM32CubeIDE and STM32CubeMX do not work properly for custom BLE profiles in the STM32WB55. When will the tools support it, and when will the documentation be updated with the current system?Firstly, I would prefer ...
I have made my own board using the STM32WB55CGU processor (the 48 pin package, as used on the Nucleo Dongle, MB1293C.I am now trying to get the BLE working and tuned. The first step, it seems, is to load the transparent mode firmware into the chip wh...
I am using the STM32WB55 Nucleo board and the firmware pack (currently at 1.7.0) includes examples for the standard set of IDEs (EWARM,MDK-ARM & SW4STM32). I can import the SW4 project into the STM32CubeIDE, but it does not retain the link to the Cu...
Kudos from