NUCLEO-WBA25CE1 "Bootloader limitation"
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.
Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.
Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link MATTER - Matter software expansion for STM32Cube - STMicroelectronics It is a reference implementation for the demonstration of Matter on ST...
Please go and visit our wiki pages where you can find a lot of information on our wireless product families (WB, WBA, WL) and the supported protocols: BLE, Zigbee, Thread, Matter, Lora, ... To begin your technical journey, please start from this top ...
I am using TrueStudio as my IDE, so had to port the files from the example into a TrueStudio project. After a lot of work i gotten the project to build and run on the p-nucleo wb55. But when i connect to the HRSTM thorugh the ST BLE Sensor app on my ...
I just received STM32WB55 Nucleo pack. I'm going through the instructions in Projects/STM32WB_Copro_Wireless_Binaries/Release_Notes.html.All going fine until I get to step 4:0x20030030 : 00050300 : FUSv0.5.3 => Must be updated using STEP 5.Next I ru...
Goodday, would you mind advice me pls if this module GPS Development Tools STEVAL-STRKT01 LoRa IoT tracker can work standlone powered with a battery.. i need to track an hobbyists drone and my per car. which program on smartphone or pc can be use?
Hi thereI am currently developing a product and i would like to use either stmb32wb55ce or stm32wb55rgI have done most of the softwaredevlopment on the nucleo board with stm32wb55rg.I am a bit stuck with the analog world on this MCU.I would like to u...
how to plugin STM32WB software to stm32CubeMX?
Hello, I want to use the last page of the flash memory.The last page of the STM32WB55CG is page 255 @ 0x080F F000 - 0x080F FFFF, 4 K, Page 255But, when I look at memory window, during run-time, I see there is nothing.See attached picwhere is the memo...
The reason for the question is to locate all errors and warnings into a single function so as not to have error handler fuctions located in several places in the code. does anyone have this request previously implemented and can give some input here....
I am looking for application notes with sample code to configure and setup Interrupt Service Routines using the NVIC of the CortexM4 in the STM32WB55.thanks
I am trying to use STM32CubeMonitor-RF to tune the HSE of a custom board but cannot find the script files needed to follow the example procedure outlined in the documentation (https://www.st.com/content/ccc/resource/technical/document/application_not...
I am issuing the following commands via USB:!deviceeui=323732385C377408!joineui=70B3D57ED002B102!appkey=DA7D3CC452FB6DEBEE88FBE8E40E0925!sysreset--Wait for reset --?devicejoinparamThe unit prints out the old info and never updates with the new keys. ...