STM32 MCUs Wireless

Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NUCLEO-WBA25CE1 "Bootloader limitation"

Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.

ctrois by ST Employee
  • 267 Views
  • 1 replies
  • 2 kudos

Matter software expansion for STM32Cube

Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link  MATTER - Matter software expansion for STM32Cube - STMicroelectronics  It is a reference implementation for the demonstration of Matter on ST...

Ouadi by ST Employee
  • 4096 Views
  • 0 replies
  • 3 kudos

How create devEUI for public Lora network?

I have one product with inside the module Murata CMW. The product will be present on a public Lora network. The product is a sensor, so it will trasmit dataI need to go in mass production and I need to create the devEUI for each deviceHow I can creat...

FSogn by Associate
  • 2354 Views
  • 2 replies
  • 0 kudos

STM32WL55 as single chip 4-fsk transceiver

Hi, I'd like to understand how I can setup the semtech transceiver to work with 4-FSK modulation. I configured a project in cube mx but I have doubts on the bandwidth and datarate parameters.I know that my datarate is 9600 bps, then bandwidth and cod...

ltoso.1 by Associate II
  • 2361 Views
  • 2 replies
  • 0 kudos

MOOC - STM32WL workshop - 4 Point to point

First of all, I was doing basic HAL_UART communication with lora modules. Now I have a new project which requires really really low power so I decided to go with stm32wl.I will have 50 end node device (sensor device) and 1 base station. Sensor device...

AHakk.1 by Associate III
  • 1212 Views
  • 1 replies
  • 0 kudos

STM32WLE5 'Failure To Execute Command'

I am experimenting with the STM32WLE5 and the embedded SX126 LoRa-radio. (aka SubGHz)I simply reset the SubGHz, then read its status, and this always returns a 'Failure To Execute Command' (according to section 13.5.1 GetStatus from SX126 datasheet) ...

Strooom by Senior
  • 4344 Views
  • 6 replies
  • 0 kudos

ISSUE: STM32WL55JC2 SPI1 not working when project file is generated from CubeMX but works while using example file.

Hello,Currently I am working on STM32WL55JC single core where I initialized PB3, PB4, PB5 and PA15 for SPI1 line with a FLASH Memory MT25QL.I tried basic with reading Flash memory ID.It worked when i used the SPI_FullDuplex_ComPolling_Master example ...

0693W00000aHUUtQAO.png 0693W00000aHUZYQA4.png
SSaya.1 by Associate II
  • 3598 Views
  • 5 replies
  • 0 kudos

Child joins openthread network late

Hello everybody .I am using openthread in a project. I am creating an openthread network using the stm32wb processor. I install the MTD stack software on the slaves I choose from my cards because I always want them to be child. Everything works fine,...

Mtopa.1 by Associate II
  • 926 Views
  • 0 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.