STM32 MCUs Wireless

Ask questions and discuss STM32 wireless solutions and their implementation for running Bluetooth LE, Zigbee, LoRaWAN applications.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NUCLEO-WBA25CE1 "Bootloader limitation"

Hi, As per UM3610 « section 7.7 », a "Bootloader limitation" has been found in NUCLEO-WBA25CE1. Please refer to "Workaround" section if you are facing this limitation.

ctrois by ST Employee
  • 218 Views
  • 1 replies
  • 1 kudos

Matter software expansion for STM32Cube

Dear all, The X-CUBE-MATTER Expansion Package is now available on our official website following this link  MATTER - Matter software expansion for STM32Cube - STMicroelectronics  It is a reference implementation for the demonstration of Matter on ST...

Ouadi by ST Employee
  • 4064 Views
  • 0 replies
  • 3 kudos

We have an STM32WL55 processor. The FLASH memory is divided for two cores: CM0PLUS FLASH (rx) : ORIGIN = 0x08020000, LENGTH = 128K CM4 FLASH (rx) : ORIGIN = 0x08000000, LENGTH = 128K Everything works.

But we need to increase the memory for CM4, so we modified the files STM32WL55CCUX_FLASH.ld:CM0PLUSFLASH (rx) : ORIGIN = 0x08030000, LENGTH = 64KCM4FLASH (rx) : ORIGIN = 0x08000000, LENGTH = 192KUnfortunately, it stopped working with this definition....

JHave.1 by Associate II
  • 1445 Views
  • 1 replies
  • 0 kudos

Testing the BLE_DataThroughput application

I'm trying to check the dependence of BLE data rate with respect to distance from the board. I runned the BLE_DataThroughput example but I'm having a hard time to interpret the info on the gatt_server terminal (I'm using a nucleo board with a smartph...

Kolab by Senior
  • 2813 Views
  • 3 replies
  • 0 kudos

Resolved! MB1791 Development Board PCB Layout

Beside the MB1791 BOM doubt, there is PCB Layer Stack doubt too.About MB1791 PCB & Gerber Files, there is no Signal copper layout in the Middle Layer-1 (G1 Layer) & Middle Layer-2 (G2 Layer). Why the setting applied 4-layers PCB instead of 2-layers ...

KKan.1 by Associate II
  • 1346 Views
  • 1 replies
  • 0 kudos

Resolved! LoRa without LoRaWAN??

Hello all....New to the STM32WL world and trying to understand some things:Could someone point me to the appropriate applications, within the STM32WL Library package framework, for creating a remote control hub that could send a user defined packet s...

SWenn.1 by Senior III
  • 2442 Views
  • 2 replies
  • 0 kudos

Hardware Difference between LRWAN_GS_HF1 and LF1?

Hello I bought the P-NUCLEO-LRWAN3 developer board to use as a gateway for lorawan.Only to realise that its meant for 433MHz, and I need 868MHz.As far as can see there is little difference between the 2 versions.Its the same PCB, so I was wondering ...

STM32WLx5 FCC RF modules?

The WL product has been around for a while now and I still only see one FCC approved RF module (Seeed )......I had heard that ST was going to produce an FCC module with the WL55 product. Can anyone from ST validate any truth to this and comment on t...

SWenn.1 by Senior III
  • 1011 Views
  • 0 replies
  • 0 kudos