User Activity

I use a GNSS connected to LPUART and a LoRaWAN module connected to USART1.I use the two UARTs via the RXNE interrupt.If I initialise and enable the two UART interrupts, USART1 no longer interrupts me and I do not receive any data. The problem is only...
I'm using the STACK "stm32wb5x_Mac_802_15_4_fw.bin"on the STM32WB55 and in principle it works correctly.The problem is that after a few hours and after having been working correctly it seems that the cortex-M0 does not answer to the cortex M4 and I g...
I am using the STM32WB55 microcontroller where I use BLE and integrate my main program with code that I am implementing.On the other hand, I need to use LoRaWAN and for this I use the HOPERF RFM95 module in which only the radio part is integrated but...
Kudos from